MBDT 1.4, S32k358, ADC not reading anything

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MBDT 1.4, S32k358, ADC not reading anything

199 次查看
primo
Contributor I

Hello to all NXP community,

I am currently working with the ADC reading on the S32k358 to achieve the closed loop current control on the contactor driver. However, I was unable to retrieve any readings from the ADC port.

The ADC port that I am using is the PTE_21 and PTE_2. I have enabled the interrupt in Platform section, defined AdcHwUnit, AdcHwTrigger, and BctuHwUnit. The clock in the MCU section is also enabled. I tried to stick to the configuration pattern in the example for S32k396 (ADC CTU S32k396). However, the interrupt callback is not triggered once and there is no ADC value. I tried the same way with the single read example, still nothing working.

Considering that there is not error when compiling, I am assuming this is is a software issue, but i could not tell where was wrong or missing. The matlab code snippet is attatched in the screenshot. I have also included the configuration file if that helps.

Thank you for your patience.

Sincerely

Primo

primo_0-1719981842034.pngprimo_1-1719981866541.pngprimo_2-1719981980547.png

 

0 项奖励
回复
0 回复数