参考文档上有下面这句话:
1.2.5 Setting the Path for Model Based Design Toolbox
For MALAB to recognize the Model Based Design Toolbox, the path needs to be setup in the
MATLAB environment. This is done by navigating the MATLAB Current Directory to the
MBD Toolbox/mbdtbx_S32K installation directory and running the “mbd_s32k_path”
script.
>> mbd_s32k_path
Treating 'D:\MBD_Toolbox\mbdtbx_S32K' as MBD Toolbox installation
root.
MBD Toolbox path prepended.
Successful.
>>
不知道如何操作的?
Ni Hao,
I'm not sure if I've understood your question correctly but here are the steps you need:
#1: Go to the folder where the mbd_s32K_path.m file exists
#2: Right click on the file and select RUN
#3: In the MATLAB command line you should be able to see:
If you need to check if the NXP Toolbox has been added to the MATLAB paths, then please use the Set Path button to open the available paths dialogue:
Hope this helps!
Daniel
Get it , Thanks!