How to update from v4.1.0 to v.4.2.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to update from v4.1.0 to v.4.2.0?

Jump to solution
642 Views
juliana_rojas30
Contributor III

Hello there!

I have a pretty basic question. I want to update my toolbox from V4.1.0 to v4.2.0, but I am not sure which file to download or how to do it. I see the files in the image below, which one should I use?

img1.PNG

Should I uninstall the previous installation and start from zero with the new one? Or can I install it on the old version? How should I proceed? Some help would be really appreciated!

Thank you all!

0 Kudos
1 Solution
626 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @juliana_rojas30 ,

The best way is to uninstall the 4.1.0 version. For that, you can delete the files from the AddOns folder on the Matlab version and then reset Matlab's path to default.

Then you can install the 4.2.0. You can do this directly from Matlab's Add-Ons following the instructions there. 

mariuslucianand_0-1610365981992.png

Hope this helps,

Marius

View solution in original post

0 Kudos
1 Reply
627 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @juliana_rojas30 ,

The best way is to uninstall the 4.1.0 version. For that, you can delete the files from the AddOns folder on the Matlab version and then reset Matlab's path to default.

Then you can install the 4.2.0. You can do this directly from Matlab's Add-Ons following the instructions there. 

mariuslucianand_0-1610365981992.png

Hope this helps,

Marius

0 Kudos