HOW TO WORK TD HANDLER BLOCKS(MBDT)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HOW TO WORK TD HANDLER BLOCKS(MBDT)

556件の閲覧回数
yavuzklcc
Contributor III

Hello everyone,

I'm reviewing the HVBMS MATLAB codes for S32K344. What I observe here is that when I provide a start location value, let's say 3, to the TD Handler functions, it allows me to read the cell voltage of the 1st cell. However, when start location is set to 10, 11, or 12, it has been used to measure the cell voltages of cells 5, 6, and 7, and also defined as faults. As seen in the photos, what I actually want to ask is that I don't know exactly what these functions do internally. I am attempting to measure temperatures from the GPIO pins of MC33775A. How can I learn about what these functions measure for each start location?

What is the fundamental operating principle of these functions?

How can I perform temperature measurement from the GPIO pins of MC33775A?

Thank you.

With best regards...

0 件の賞賛
返信
1 返信

525件の閲覧回数
yavuzklcc
Contributor III

Lastly, what I would like to inquire about is within the InsertPhyEvent block, there is a "message td" with settings configured through external configuration. It states which message to send and how to interpret the response. How can I discern which message to send and how to understand the corresponding response?

0 件の賞賛
返信