Hi,
I'm trying to use the Simulink toolbox in order to receive with my NXP S32K144 CAN message from a NXP S32K146. I'm sure that the transmitter (S32K146) works because my CANoe can read the messages sent on the bus.
I already tried the examples presented in Simulink but none of them seem to work. It seems that there are some configuration problem but I can understand what it is. The only examples I could found is https://www.nxp.com/pages/introducing-the-can-communication-blocks-from-nxp-mbdt:TIP-INTRODUCING-THE....In this examples just a virtual CAN bus is used but it doesn't work with a real CAN bus.
I attached here the last data block scheme that I'm using and the wiring between the two boards.
I already tried to use a block can receiver without interrupt but it doesn't work.
Thank you for the support