hi, i use mqx 4.2, cw 10.6 and frmk64f.
when i use this board for a comunication on ethernet lan i see that there are a lot of retransmission packets: about 30% of transmitted packet. i try to write a simple application that send several packets on lan from my board to my pc at hercules application. while it is transfering i use wireshark to see the traffic on the lan. my question is:
- is it normal to have about 30% of ethernet traffic composed by [TCP RETRANSMISSION] packets?
- there is a way to avoid it?
thanks
已解决! 转到解答。
Hi Emanuele,
please set _TCP_rto_min value to 250 just after RTCS_create().
error = RTCS_create();
_TCP_rto_min = 250;
This issue is related to Retransmission's Time Out (RTO) and Retransmission-Time Trip (RTT). I will write a small document explaining the details.
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi carlos,
i did another test but i see always the retransmission packets. i do this:
i create a new bsp cloned from frdmk64f not modified bsp
i created a new projet mqx4.2 starting from example: eth_to_serial
i replace the demo.c file with the same file i sent you
i set the bsp with ENABLE_ITTYA and ENABLE_IO_SUBSYSTEM
i compiled bsp, psp and rtcs lib.
i compiled the code
i run on my device and i see always the retransmission packet.
is it possible?
are you using a not modified version of frdmk64f bsp?