hi, i use mqx 4.2, cw 10.6 and frmk64f.
when i use this board for a comunication on ethernet lan i see that there are a lot of retransmission packets: about 30% of transmitted packet. i try to write a simple application that send several packets on lan from my board to my pc at hercules application. while it is transfering i use wireshark to see the traffic on the lan. my question is:
- is it normal to have about 30% of ethernet traffic composed by [TCP RETRANSMISSION] packets?
- there is a way to avoid it?
thanks
已解决! 转到解答。
Hi Emanuele,
please set _TCP_rto_min value to 250 just after RTCS_create().
error = RTCS_create();
_TCP_rto_min = 250;
This issue is related to Retransmission's Time Out (RTO) and Retransmission-Time Trip (RTT). I will write a small document explaining the details.
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Emanuele,
please set _TCP_rto_min value to 250 just after RTCS_create().
error = RTCS_create();
_TCP_rto_min = 250;
This issue is related to Retransmission's Time Out (RTO) and Retransmission-Time Trip (RTT). I will write a small document explaining the details.
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Emanuele,
here you go TCP Retransmission Time Out (RTO) and Round-Trip Time (RTT) in MQX RTCS
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Emanuele,
Re-transmission packets usually occur when the "other side" is faster that the MCU, please consider that the MCU is relatively slow compared with other systems.
If this is the case the other side will ask for retransmission before the MCU is able to process the packet. This is way you may see many retrasmission packets.
Best regards,
Carlos
for a better explanation of the problem i need to precise that:
- the much of communication is from the MCU towards pc application.
- the retransmission is often preceded from a out-of-order packet.
this is the screenshot of a casual page on a wireshark while the communication is on.
do you think that the problem is the same in this case too?
Hi Emanuele,
sorry for the delay.
- It is true that he MCU (192.168.11.202) is slower and cannot process all packets that PC (192.168.11.1) sends and it needs to ask for retransmission. However it is not that slow to loose all the packets shown in the capture you sent.
Please review the priority of your tasks. Which is the highest priority (lower number) you set? Note that all your tasks must have a lower priority (higher number) than the tcp/ip task. If there is another task with higher priority the tcp/ip task would be blocked and unable to process the TCP packets.
Best regards,
Carlos
Hi Carlos,
the RTCS task have the default priority, that is equal to 6. The other task i use have lower priority like as 9 or 10.
I try to set an higher priority for RTCS task by set _RTCSTASK_priority=?; before RTCS_create(); call.
I see in wireshark the same behaviour with same number of retransmission packets if the RTCS task priority is set to 2, (i tried with priority 3, 4 and 5 but i see no change). The priority setting is correct because i see in the debugger, at task summary, the value i set.
Hi Emanuelle,
If you own tasks have priority of 9 and 10 then it is OK. The problem should be other.
Probably the issue is that there are many collisions. Can you please send a full capture but connecting the MCU directly to the PC please? Without any router or switch between. It is important to confirm if that the MCU is working properly in this condition.
Regards,
Carlos
Hi Emanuele,
you are using FRDM-K64 right? Can you please share your project to test it on our side?
If you prefer to share it in a private channel please enter a ticket in www.nxp.com/support under Hardware & Software category.
Please also provide instructions to reproduce the issue.
Regards,
Carlos
Hi Carlos,
the forum (or the pc) does not allow me to answer correctly and attach the file so i copy the code here.
this code shows the problem of the retransmissions.
to run this example i have this pc lan setting ip:192.168.11.1 ; subnet 255.255.255.0; gateway 192.168.11.1.
the board is connected to the pc throught a rj45 lan cable. when the application is running i use hercules to connect to the device: i choose TCP client, i set the ip of the device 192.168.11.202 , 8000 port; i set hercules to log the received info in a file because it break sometimes. when the transfer start i see in wireshark a correct communication for few seconds, then i start to see the retransmissions packets.
the code is:
#include <mqx.h>
#include <bsp.h>
#include <rtcs.h>
#if !PLATFORM_SDK_ENABLED
#include <enet.h>
#endif
#include <ipcfg.h>
#include <lwevent.h>
#include <mutex.h>
#ifndef DEMO_PORT
#define DEMO_PORT IPPORT_TELNET
#endif
#if MQX_USE_IO_OLD
#define SERIAL_DEVICE BSP_DEFAULT_IO_CHANNEL
#else
#define SERIAL_DEVICE "tty:"
#endif
/* EOF */
#define DEMOCFG_USE_WIFI BSP_ENET_WIFI_ENABLED /* USE WIFI Interface */
#define SERIAL_SOCKET_BUFFER_SIZE 1460
#ifndef ENET_IPADDR
#define ENET_IPADDR IPADDR(192,168,11,202)
#endif
#ifndef ENET_IPMASK
#define ENET_IPMASK IPADDR(255,255,255,0)
#endif
#ifndef ENET_IPGATEWAY
#define ENET_IPGATEWAY IPADDR(192,168,11,1)
#endif
#define REMOTE_PORT 50001
#ifndef ENET_MAC
#define ENET_MAC {0x00,0xA7,0xC5,0xF1,0x11,0x90}
#endif
#if PLATFORM_SDK_ENABLED
#include "app_mqx.h"
#else
#if ! BSPCFG_ENABLE_IO_SUBSYSTEM
#error This application requires BSPCFG_ENABLE_IO_SUBSYSTEM defined non-zero in user_config.h. Please recompile BSP with this option.
#endif
#ifndef BSP_DEFAULT_IO_CHANNEL_DEFINED
#error This application requires BSP_DEFAULT_IO_CHANNEL to be not NULL. Please set corresponding BSPCFG_ENABLE_ITTYx to non-zero in user_config.h and recompile BSP with this option.
#endif
#define MAIN_TASK_INDEX 1
#define RX_TASK_INDEX 2
#define TX_TASK_INDEX 3
#define WRITE_BUFFER_TASK_INDEX 4
#endif
#define SOCKET_WELCOME_MESSAGE "Ethernet <-> Serial bridge\n\r"
#define SERIAL_WELCOME_MESSAGE "Serial <-> Ethernet bridge\n\r"
#define RX_BUFFER_SIZE 128
#define TX_BUFFER_SIZE 128
#define TCP2SER_TRANSPARENT_SERVER_TASK_ID 0x3001
#define TCP2SER_TRANSPARENT_SERVER_TX_TASK_ID 0x3002
#define TCP2SER_CTRL_TASK_ID 0x3003
#define TCP2SERIAL_SERVER_PORT 8000
#define TCP2SERIAL_RESET_SOCK_TIME 300000
#define TCP2SERIAL_MAX_CLIENT_CONNECTIONS 3
#define TCP2SER_SOCKETS_NUMBER (1+TCP2SERIAL_MAX_CLIENT_CONNECTIONS+1) //server socket + client sockets + temp socket
#define TCP2SER_RX_BUF_SIZE 24
#define SER2TCP_BUF_SIZE 2920//128
#define PRINTF_DEBUG_TCP2SER if(1)fprintf
//tx
#define PRINTF_DEBUG_REMOTE_CLIENT if(1)fprintf
#define REM_CMD_BUF_MAX_SIZE 48
#define PREAMBLE_BUFF_SIZE (31)
/* Structure with sockets used for listening */
typedef struct socket_s
{
uint32_t sock6; // socket for IPv6
uint32_t sock4; // socket for IPv4
}SOCKETS_STRUCT, * SOCKETS_STRUCT_PTR;
/* Paramter for tasks */
typedef struct t_param
{
uint32_t sock;
unsigned char i;
}TASK_PARAMS, * TASK_PARAMS_PTR;
FILE_PTR debug_uart;
#if !PLATFORM_SDK_ENABLED
//MUTEX_STRUCT tcp2sersockets_mutex;
uint32_t TCP2SERsockets[TCP2SER_SOCKETS_NUMBER]={0};
sockaddr TCP2SERaddresses[TCP2SER_SOCKETS_NUMBER]={0};
uint16_t sockaddr_len;
#define TCP2SERservsock TCP2SERsockets[0]
#define TCP2SERservaddress TCP2SERaddresses[0]
#define TCP2SERVtempsock TCP2SERsockets[TCP2SER_SOCKETS_NUMBER-1]
#define TCP2SERVtempaddress TCP2SERaddresses[TCP2SER_SOCKETS_NUMBER-1]
#define TCP2SERclientsocks(x) TCP2SERsockets[x+1]
MUTEX_STRUCT SER2TCPbuf_mutex;
unsigned char SER2TCPbuf[SER2TCP_BUF_SIZE];
uint16_t SER2TCPbuf_read_index;
uint16_t SER2TCPbuf_write_index;
uint16_t SER2TCPbuf_bytes_avail;
rtcs_fd_set sock_set;
_task_id ctrl_tid[TCP2SER_SOCKETS_NUMBER];
TASK_PARAMS task_p;
unsigned char remote_client_connected=0;
uint32_t tcpclientsock=0;
IPCFG_IP_ADDRESS_DATA my_ip_data;
LWEVENT_STRUCT SER2TCPbuf_events;
/*
** MQX initialization information
*/
void main_task (uint32_t);
void rx_task (uint32_t param);
void tx_task (uint32_t param);
void ctrl_activity_task (uint32_t param);
void write_buffer_task (uint32_t param);
//function
uint32_t chiudisocket(uint32_t sock, uint32_t abort);
void start_server_sock(void);
void SER2TCPWrite(unsigned char *buf, int len);
const TASK_TEMPLATE_STRUCT MQX_template_list[] =
{
/* Task Index, Function, Stack, Priority, Name, Attributes, Param, Time Slice */
{MAIN_TASK_INDEX, main_task, 5000, 9, "Bridge", MQX_AUTO_START_TASK, 0, 0 },
{RX_TASK_INDEX, rx_task, 5000, 10, "rxtask", 0, 0, 0 },
{TCP2SER_CTRL_TASK_ID, ctrl_activity_task, 5000, 11, "TCP2SerialControlActivityTask", 0, 0, 0 },
{WRITE_BUFFER_TASK_INDEX, write_buffer_task, 5000, 10, "wbtask", 0, 0, 0 },
{0}
};
typedef uint32_t task_param_t;
#endif
void main_task( task_param_t init_data )
{
IPCFG_IP_ADDRESS_DATA ip_data;
//uint32_t error;
_enet_address enet_addr = ENET_MAC;
uint32_t retval = 0;
_task_id rx_tid,wb_tid;
_task_id tx_tid;
int32_t err;
unsigned char i;
unsigned char t;
_mqx_uint error;
uint8_t j=0;
debug_uart = fopen(SERIAL_DEVICE, "w");
if(debug_uart==NULL){
//_task_block();
}
_io_set_handle(IO_STDERR,debug_uart);
/* Initialize RTCS */
//_RTCSTASK_priority=3;
_RTCSPCB_init = 4;
_RTCSPCB_grow = 2;
_RTCSPCB_max = 20;
_RTCS_msgpool_init = 4;
_RTCS_msgpool_grow = 2;
_RTCS_msgpool_max = 20;
_RTCS_socket_part_init = 4;
_RTCS_socket_part_grow = 2;
_RTCS_socket_part_max = 20;
error = RTCS_create();
if (error != RTCS_OK)
{
fputs("Fatal Error: RTCS initialization failed.", stderr);
_task_block();
}
ip_data.ip = ENET_IPADDR;
ip_data.mask = ENET_IPMASK;
ip_data.gateway = ENET_IPGATEWAY;
/* Initialize ethernet */
error = ipcfg_init_device(BSP_DEFAULT_ENET_DEVICE, enet_addr);
if (error != IPCFG_OK)
{
fprintf(stderr, "Fatal Error 0x%X: Network device initialization failed.\n", error);
}
/* Bind static IP address */
error = ipcfg_bind_staticip(BSP_DEFAULT_ENET_DEVICE, &ip_data);
if (error != IPCFG_OK)
{
fprintf(stderr, "Fatal Error 0x%X: IP address binding failed.", error);
}
if(ipcfg_get_ip(BSP_DEFAULT_ENET_DEVICE,&my_ip_data)){
fprintf(debug_uart,"\n\n\rethernet Bound with IP %08X\n", my_ip_data.ip);
}
_mutex_init(&SER2TCPbuf_mutex,NULL);
_lwevent_create(&SER2TCPbuf_events,0);
start_server_sock();
RTCS_FD_ZERO(&sock_set);
RTCS_FD_SET(TCP2SERservsock,&sock_set);
rx_tid=_task_create(0,RX_TASK_INDEX,0);
wb_tid=_task_create(0,WRITE_BUFFER_TASK_INDEX,0);
/*while(1){
_time_delay(1000);
}*/
while(1){
err=select(1,&sock_set,NULL,NULL, 0);//err=RTCS_selectset(TCP2SERsockets,TCP2SER_SOCKETS_NUMBER,0);
if(err==RTCS_ERROR){
//manage error
PRINTF_DEBUG_TCP2SER (debug_uart,"\n\rtrasparent_8000 RTCS error");
err=RTCS_get_errno();
PRINTF_DEBUG_TCP2SER(debug_uart, ": %X\n\r",err);
_task_abort(tx_tid);
for (i=0;i<TCP2SER_SOCKETS_NUMBER;i++) {
if (TCP2SERsockets[i]!=0) {
err=chiudisocket(TCP2SERsockets[i],0);//shutdown(TCP2SERsockets[i],FLAG_CLOSE_TX);
if(err!=RTCS_OK){
fprintf(debug_uart, "\n\rtrasparent_8000: rtcs shutdown %d err: 0x%X\n\r",i,err);
//manage
}
RTCS_FD_CLR(TCP2SERsockets[i],&sock_set);
TCP2SERsockets[i]=0;
if (i!=0) {
if (_task_abort(ctrl_tid[i])==MQX_OK) {
PRINTF_DEBUG_TCP2SER (debug_uart,"\n\rtrasparent_8000 trasp, rtcs_err aborting ctrl task %d", i);
}
}
}
}
_time_delay(200);
start_server_sock();
RTCS_FD_ZERO(&sock_set);
RTCS_FD_SET(TCP2SERservsock,&sock_set);
}
else if(err==0){//timeout
PRINTF_DEBUG_TCP2SER (debug_uart,"\n\rtrasparent_8000 RTCS timeout 8000:");
}
else{//activity
if(RTCS_FD_ISSET(TCP2SERservsock, &sock_set)){//if(err==TCP2SERservsock){//new connection request
//fprintf(stderr,"\n\rtrasparent_8000 Server activity\n\r");
sockaddr_len=sizeof(TCP2SERVtempaddress);
TCP2SERVtempsock=accept(TCP2SERservsock, &TCP2SERVtempaddress, &sockaddr_len);
if(TCP2SERVtempsock==RTCS_SOCKET_ERROR){
fprintf(stderr,"\n\rtrasparent_8000 Server error\n\r");
retval = RTCS_geterror(TCP2SERservsock);
if (retval == RTCS_OK) {
printf("\n\rtrasparent_8000 Connection reset by peer");
} else {
printf("\n\rtrasparent_8000 Error, accept() failed with error code %x",retval);
}
}
else{
for(i=1;i<=TCP2SERIAL_MAX_CLIENT_CONNECTIONS;i++){
if(TCP2SERsockets[i]==0){
break;
}
}
if(i>TCP2SERIAL_MAX_CLIENT_CONNECTIONS){//no connections available
//refuse connection
chiudisocket(TCP2SERVtempsock,0);//shutdown(TCP2SERVtempsock,FLAG_CLOSE_TX);
TCP2SERVtempsock=0;
fprintf(stderr,"\n\rtrasparent_8000 Connection refused\n\r");
}
else{
//Connection is maintained and handle saved
t=TRUE;
setsockopt(TCP2SERVtempsock,SOL_TCP,OPT_RECEIVE_NOWAIT,&t,1);
TCP2SERsockets[i]=TCP2SERVtempsock;
TCP2SERaddresses[i]=TCP2SERVtempaddress;
TCP2SERVtempsock=0;
fprintf(stderr,"\n\rtrasparent_8000 : Accepted connection by %08X, port %d\n\r",TCP2SERaddresses[i].sin_addr.s_addr,TCP2SERaddresses[i].sin_port);
task_p.i = i;
task_p.sock = TCP2SERsockets[i];
ctrl_tid[i]=_task_create(0,TCP2SER_CTRL_TASK_ID, &task_p);
if (ctrl_tid == MQX_NULL_TASK_ID){
fprintf(stderr, "\n\rtrasparent_8000 Impossible to start ctrl task");
}
}
}
}
}
_time_delay(1);
}
}
void rx_task (uint32_t param)
{
unsigned char i;
int32_t ret;
int32_t len;
unsigned char tx_buf[(SER2TCP_BUF_SIZE/2)]={0};
uint16_t tx_buf_index=0;
PRINTF_DEBUG_TCP2SER (debug_uart,"\n\rtrasparent_8000 trasparent task on");
_mqx_uint error;
while(1){
//_lwevent_wait_ticks(&SER2TCPbuf_events,0x02,TRUE,200);
_mutex_lock(&SER2TCPbuf_mutex);
tx_buf_index=0;
while(SER2TCPbuf_bytes_avail>0){
tx_buf[tx_buf_index++]=SER2TCPbuf[SER2TCPbuf_read_index++];
SER2TCPbuf_bytes_avail--;
if(SER2TCPbuf_read_index>=SER2TCP_BUF_SIZE){
SER2TCPbuf_read_index=0;
}
if(tx_buf_index>=(SER2TCP_BUF_SIZE/2)){//64){
break;
}
}
_mutex_unlock(&SER2TCPbuf_mutex);
for(i=0;i<TCP2SERIAL_MAX_CLIENT_CONNECTIONS;i++){
if(TCP2SERclientsocks(i)!=0){
ret=send(TCP2SERclientsocks(i),tx_buf,tx_buf_index,0);
if (tx_buf_index!=0) {
PRINTF_DEBUG_TCP2SER(debug_uart,"\n\rtcp2ser SENT:%d bytes to TCP", tx_buf_index);
}
if(ret==RTCS_ERROR){
ret=RTCS_geterror(TCP2SERclientsocks(i));
chiudisocket(TCP2SERclientsocks(i),0);
//if(ret==RTCSERR_SOCK_INVALID){
TCP2SERclientsocks(i)=0;
//}
fprintf(stderr,"tcp2ser trasp tx, RTCS ERR: %x",ret);
}
}
}
_time_delay(1);
}
}
uint32_t chiudisocket(uint32_t sock, uint32_t abort){
struct linger l_options = {0};
uint32_t ret=0;
int32_t mode=0;
int32_t err=0;
//hard close
mode=(int32_t)abort;
// Set linger options for RST flag sending.
l_options.l_onoff = mode;//1=abort, 0=graceful
//l_options.l_linger_ms = 0;
err=setsockopt(sock, SOL_SOCKET, SO_LINGER, (const void*)&l_options, sizeof(l_options));
if (err == RTCS_OK) {
err=closesocket(sock);
}
ret=(uint32_t)err;
return(ret);
}
void start_server_sock(void) {
uint32_t errval;
TCP2SERservsock=socket(PF_INET, SOCK_STREAM, 0);
if (TCP2SERservsock == RTCS_SOCKET_ERROR){
fputs("\n\rtrasparent_8000 Error: Unable to create socket for IPv4 connections.", stderr);
//_task_block();
}
PRINTF_DEBUG_TCP2SER (debug_uart,"\n\rtrasparent_8000 created srv sock 0x%X", TCP2SERservsock);
((sockaddr_in*) &TCP2SERservaddress)->sin_family = AF_INET;
((sockaddr_in*) &TCP2SERservaddress)->sin_port = TCP2SERIAL_SERVER_PORT;
((sockaddr_in*) &TCP2SERservaddress)->sin_addr.s_addr = INADDR_ANY;
errval = bind(TCP2SERservsock, &TCP2SERservaddress, sizeof(TCP2SERservaddress));
if(errval != RTCS_OK){
//_task_block();
}
errval = listen(TCP2SERservsock, 0);
if (errval == RTCS_OK){
fprintf(stderr,"\n\rtrasparent_8000 SERV listening on 8000\n\r");
}
else{
//_task_block();
}
}
void ctrl_activity_task (uint32_t param) {
uint32_t sockets_array[2] = {0};
uint32_t err = 0;
unsigned char j = 0;
rtcs_fd_set sock_ctrl_set;
unsigned char tcp_rx_buf[TCP2SER_RX_BUF_SIZE];
j = ((TASK_PARAMS_PTR)param)->i;
sockets_array[0] = ((TASK_PARAMS_PTR)param)->sock;
RTCS_FD_ZERO(&sock_ctrl_set);
RTCS_FD_SET(sockets_array[0],&sock_ctrl_set);
PRINTF_DEBUG_TCP2SER (debug_uart,"\n\rtrasparent_8000 start ctrl task for %d sock 0x%x ", j, sockets_array[0]);
while(1){
err=select(1,&sock_ctrl_set,NULL,NULL,TCP2SERIAL_RESET_SOCK_TIME);//err=RTCS_selectset(sockets_array, 1 , TCP2SERIAL_RESET_SOCK_TIME);
if(err==RTCS_ERROR){
//manage error
err = RTCS_get_errno();
PRINTF_DEBUG_TCP2SER (debug_uart,"\n\rtrasparent_8000 ctrl rtcs error is: 0x%x ", err);
err=chiudisocket(sockets_array[0],0);
if(err!=RTCS_OK){
fprintf(debug_uart, "\n\rtrasparent_8000 ctrl: Shutdown %d err: 0x%X\n\r",j,err);
//manage
} else {
PRINTF_DEBUG_TCP2SER (debug_uart, "\n\rtrasparent_8000 ctrl: Shutdown sock %d: 0x%X\n\r",j,err);
TCP2SERsockets[j]=0;
}
//End of operations - task kills itself
_task_abort(_task_get_id());
}
else if(err==0){//timeout
PRINTF_DEBUG_TCP2SER (debug_uart,"\n\rtrasparent_8000 ctrl RTCS timeout 8000:");
err=chiudisocket(sockets_array[0],0);
if(err!=RTCS_OK){
fprintf(debug_uart, "\n\rtrasparent_8000 ctrl: Shutdown %d err: 0x%X\n\r",j,err);
//manage
} else {
PRINTF_DEBUG_TCP2SER (debug_uart, "\n\rtrasparent_8000 ctrl: Shutdown sock %d: 0x%X\n\r",j,err);
TCP2SERsockets[j]=0;
}
_task_abort(_task_get_id());
} else {
if (RTCS_FD_ISSET(sockets_array[0], &sock_ctrl_set)){
err=recv(sockets_array[0], tcp_rx_buf, TCP2SER_RX_BUF_SIZE, 0);
if(err==RTCS_ERROR){
err = RTCS_geterror(sockets_array[0]);
PRINTF_DEBUG_TCP2SER (debug_uart,"\n\rtrasparent_8000 ctrl: recv error for sock %X, is: 0x%x ",sockets_array[0], err);
fprintf(stderr,"\n\rtrasparent_8000 ctrl: Shutting down sock %d",j);
err=chiudisocket(sockets_array[0],0);
if(err!=RTCS_OK){
fprintf(debug_uart, "\n\rtrasparent_8000 ctrl: Shutdown %d err: 0x%X\n\r",j,err);
//manage
}
TCP2SERsockets[j]=0;
_task_abort(_task_get_id());
}
else if(err!=0){
fprintf(debug_uart, "\n\rtrasparent.8000 ctrl Received %d bytes\n",err);
//SerialTxTransparent(tcp_rx_buf,err);
} else if (err==0){
PRINTF_DEBUG_TCP2SER (debug_uart,"\n\rtrasparent_8000 ctrl, err=0");
}
}
}
_time_delay(1);
}
}
void write_buffer_task (uint32_t param){
unsigned char source_buf[SER2TCP_BUF_SIZE]={0};
int buf_len=10;
uint8_t val=0;
uint16_t count=0;
source_buf[1]=0x01;
fprintf(debug_uart, "\n\rstart write buffer task");
while(1){
for (uint8_t l=0;l<10;l++){
for (uint8_t k=0;k<12;k++){
SER2TCPWrite(source_buf,buf_len);
//_time_delay(50);
}
_time_delay(100);
}
fprintf(debug_uart, "\n\rwrite buffer cycle");
_time_delay(100);
}
}
void SER2TCPWrite(unsigned char *buf, int len){
int n;
_mutex_lock(&SER2TCPbuf_mutex);
for(n=0;n<len;n++){
SER2TCPbuf[SER2TCPbuf_write_index++]=buf[n];
if(SER2TCPbuf_write_index>=SER2TCP_BUF_SIZE){
SER2TCPbuf_write_index=0;
}
if(SER2TCPbuf_bytes_avail<SER2TCP_BUF_SIZE){
SER2TCPbuf_bytes_avail++;
}
else{//buffer is already full - overwrites older bytes
SER2TCPbuf_read_index++;
if(SER2TCPbuf_read_index>=SER2TCP_BUF_SIZE){
SER2TCPbuf_read_index=0;
}
}
}
if(SER2TCPbuf_bytes_avail>0){
_lwevent_set(&SER2TCPbuf_events,0x01);
}
if(SER2TCPbuf_bytes_avail>=16){
_lwevent_set(&SER2TCPbuf_events,0x02);
}
_mutex_unlock(&SER2TCPbuf_mutex);
}
Hi Emanuele,
you can send me the project to Carlos.Musich@nxp.com
Please clean the project (menu Project > Clean) and DO NOT compile it, then zip it and send it. If you build the project all object code and debug symbols are generated which cause the project to be SO heavy.
Regards,
Carlos
hi Carlos,
for this project i start with the example eth_to_serial from RTCS examples. if you copy the code in demo.c file and maybe set some project configuration i think it should work. anyway i will send you this zip package soon.
Hi,
I configured board IP to 192.168.1.202 and it is connected to router (gateway) with IP 192.168.1.1 which provides IP address by DHCP to my PC which is 192.168.1.132. I cannot see the retransmission's packages.
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------