on NXP PCAL6416AHF,128 - I/O Expander,

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

on NXP PCAL6416AHF,128 - I/O Expander,

1,112 Views
sms1
Contributor I

Hi Nxp Team,

Please advice us on the below customer issue.@

NXP PCAL6416AHF,128 - I/O Expander, 16bit, 400 kHz, I2C, 1.65 V, 5.5 V, HWQFN URL NXP: https://www.nxp.com/part/PCAL6416AHF

ISSUE: 10 of the 25 defects. The complete circuit in which this device is used just does not work... "Dead". By replacing them with a good one the circuit works just fine. Please check the two attached images of the imprint on the devices. Defect IO chip.bmp Good.bmp

QUESTION: How to go forth with NXP? Can they recognize something by these imprints and what the possible workaround might be? Maybe a start current being slightly too high or a voltage out of a certain window?

0 Kudos
5 Replies

961 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

If so,no more issue about schematic,please contact with NXP local quality team for next failure analysis about the bad part.

0 Kudos

961 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Please show us your application circuit and environment!

Please also do a PCB failure analysis about fail boards to eliminate the solder issue.

0 Kudos

961 Views
sms1
Contributor I

Any progress on this issue...guoweisun

Hi Team,

Please find the attachments from the customer as requested.

As requested more information from the customer:

  • Pull up 1k8 on SDA and SCL lines

  • Photo of the PCB:

2019-09-30 11.03.06.jpg

  • Part of the schematic:

image004.png

  • Part of the PCB layout:

image003.png

Regards,

Siddu

M +919945211348

0 Kudos

961 Views
guoweisun
NXP TechSupport
NXP TechSupport

For your schematic:

1: do you pull up SCL/SDA to VCC?

2: What's VSS value?

0 Kudos

960 Views
sms1
Contributor I

Yes, pull up 1k8 on both lines.
VSS si in fact V5s and is 5Volt.

0 Kudos