Dear support,
I am sending data via mcc from a Vybrid M4 to an A5 using MQX (for my system data see thread 329003).
Lately I am not receiving any data on the A5 unless I first run into a breakpoint on M4 (which was arbitrarily chosen).
I wonder if this has to do with the message on the debugger which I get after halting (without breakpoint) and attempting to proceed further
Target Message: Attempt to go without Thumb state set in xPSR
ERROR(CMD441-TAD8-NAL24):
! Continuing failed
! Unable to run device Cortex-M4_0
! Bad mode for step/go.
Also on the breakpoint list after the mentioned breakpoint there is the suffix [ #1 T32(Thumb)]. Otherwise only [#1].
I would like the mcc to work without the 'breakpoint trick'. Can you help?
With best regards,
Heinz