mcc transmission only an intermediary breakpoint

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mcc transmission only an intermediary breakpoint

555 Views
heinzroitner
Contributor II

Dear support,

I am sending data via mcc from a Vybrid M4 to an A5 using MQX (for my system data see thread 329003).

Lately I am not receiving any data on the A5 unless I first run into a breakpoint on M4 (which was arbitrarily chosen).

I wonder if this has to do with the message on the debugger which I get after halting (without breakpoint) and attempting to proceed further

 

Target Message: Attempt to go without Thumb state set in xPSR

ERROR(CMD441-TAD8-NAL24):

! Continuing failed

! Unable to run device Cortex-M4_0

! Bad mode for step/go.

Also on the breakpoint list after the mentioned breakpoint  there is the suffix [ #1 T32(Thumb)]. Otherwise only [#1].

I would like the mcc to work without the 'breakpoint trick'. Can you help?

With best regards,

Heinz

0 Kudos
2 Replies

369 Views
heinzroitner
Contributor II

Dear support,

this has been a temporary debugger problem. This ssue is resolved.

But a new problem has become urgent! Please see my new thread 'mcc transmission problem'.

Thanks,

Heinz


0 Kudos

369 Views
RadekS
NXP Employee
NXP Employee

Thank you for your information


Have a great day,
RadekS

0 Kudos