Hi,
I'm currently using MQX 3.8.1 with Code Warrior 10.2 and the Kinetis k60 tower. I'm currently having trouble sending strings over multiple instances and was wondering if this was a timing issue.
My setup:
I have two tasks: connect_task and print_task.
the connect_task initializes RTCS and creates and connects a socket to an external server. My tower is acting as a client.
This task is successful because I sent a string confirming connection and verified that the server was able to receive it, so I know that the connection was successful and I was able to send a string over TCP/IP to a server.
Once finished it creates 5 instances of the print task and passes in 5 different strings. This is almost exactly like the mutex example provided.
the print_task is where I'm having trouble. Since I have already opened the socket, I set the same parameters and attempted to send that data the same way I did in the connect_task. I was wondering if this was a timing issue and the send was blocking.
Below is my code.
Thanks,
Khoa Nguyen
/****************************************************************************
* RYSK TECH
* RMD
* Created by: Khoa Nguyen
* Date: October 1, 2012
* Description: Demo for the CDR
****************************************************************************/
#include "main.h"
#include "mutex.h"
#if !BSPCFG_ENABLE_IO_SUBSYSTEM
#error This application requires BSPCFG_ENABLE_IO_SUBSYSTEM defined non-zero in user_config.h. Please recompile BSP with this option.
#endif
#ifndef BSP_DEFAULT_IO_CHANNEL_DEFINED
#error This application requires BSP_DEFAULT_IO_CHANNEL to be not NULL. Please set corresponding BSPCFG_ENABLE_TTYx to non-zero in user_config.h and recompile BSP with this option.
#endif
#if ! MQX_HAS_TIME_SLICE
#error This application requires MQX_HAS_TIME_SLICE defined non-zero in user_config.h. Please recompile kernel with this option.
#endif
#if ! BSPCFG_ENABLE_GPIODEV
#error This application requires BSPCFG_ENABLE_GPIODEV defined non-zero in user_config.h. Please recompile BSP with this option.
#endif
TASK_TEMPLATE_STRUCT MQX_template_list[] =
{
/* Task Index, Function, Stack, Priority, Name, Attributes, Param, Time Slice */
{ IDLE_TASK, idle_task, 2000, 7, "idle", MQX_AUTO_START_TASK, 0, 0 },
{ CONNECT_TASK, connect_task, 1000, 6, "connect", 0, 0, 0 },
{ PRINT_TASK, print_task, 1000, 9, "print", MQX_TIME_SLICE_TASK, 0, 3 },
{ 0 }
};
/*TASK*-----------------------------------------------------
*
* Task Name : Main_task
* Comments :
*
*END*-----------------------------------------------------*/
void idle_task(uint_32 initial_data)
{
/*Initialize Mutex struct and hard code 4 strings*/
MUTEX_ATTR_STRUCT mutexattr;
char* string1 = "1 Sensor ONE task\n";
char* string2 = "2 Sensor TWO task\n";
char* string3 = "3 Sensor THREE task\n";
char* string4 = "4 Sensor FOUR task\n";
/* Initialize mutex attributes */
if (_mutatr_init(&mutexattr) != MQX_OK) {
printf("Initialize mutex attributes failed.\n");
_task_block();
}
/* Initialize the mutex */
if (_mutex_init(&print_mutex, &mutexattr) != MQX_OK) {
printf("Initialize print mutex failed.\n");
_task_block();
}
printf("\n Welcome to the RYSK Tech RMD device \n");
_task_create(0, CONNECT_TASK, 0);
_time_delay(5000);
/* Create the print tasks */
_task_create(0, PRINT_TASK, (uint_32)string1);
_task_create(0, PRINT_TASK, (uint_32)string2);
_task_create(0, PRINT_TASK, (uint_32)string3);
_task_create(0, PRINT_TASK, (uint_32)string4);
_task_block();
}
void connect_task(uint_32 initial_data)
{
_ip_address ipaddr;
uint_32 sock;
uint_32 result;
sockaddr_in addr;
char* test = "This is a test for stream";
while(1)
{
if (_mutex_lock(&print_mutex) != MQX_OK)
{
printf("Mutex lock failed.\n");
_task_block();
}
rtcs_init();
addr.sin_family = AF_INET;
addr.sin_port = 10000;
addr.sin_addr.s_addr = IPADDR(192,168,3,102);
sock = socket(AF_INET, SOCK_STREAM, 0);
result = connect(sock, &addr, sizeof(addr));
//_time_delay(1000);
if(result != RTCS_OK)
{
printf("ERROR the socket could not CONNECT");
}
if(result == RTCS_OK)
{
printf("\nREADY TO SEND DATA!!!!!!!!!!!!!!!!!");
printf("\nConnected to %lx, port %d",addr.sin_addr.s_addr, addr.sin_port);
}
send(sock, (void *)test, strlen(test), 0);
_mutex_unlock(&print_mutex);
_task_block();
}
}
void print_task(uint_32 initial_data)
{
while(1)
{
_ip_address ipaddr;
uint_32 sock;
uint_32 result;
sockaddr_in addr;
char* cBuffer;
char tag[50];
char Buffer[50] ={0};
sprintf(tag, (char *)initial_data);
sprintf(Buffer, (char *)initial_data);
cBuffer = Buffer;
if (_mutex_lock(&print_mutex) != MQX_OK) {
printf("Mutex lock failed.\n");
_task_block();
}
addr.sin_family = AF_INET;
addr.sin_port = 10000;
addr.sin_addr.s_addr = IPADDR(192,168,3,102);
send(sock, (void *)Buffer, strlen(Buffer), 0);
_io_puts((char *)initial_data);
_mutex_unlock(&print_mutex);
}
}
/* EOF */
已解决! 转到解答。
Your socket handle in the print_task() is a local variable, not being initialized.
I think you should make the sock variable (socket handle) global, so that when you initialize it in the connect_task, you can refer to it from the print_task(s).
Right now, the sock variable in the print_task() is undefined value on the print_task's stack, so you can't send() via undefined socket.
Your socket handle in the print_task() is a local variable, not being initialized.
I think you should make the sock variable (socket handle) global, so that when you initialize it in the connect_task, you can refer to it from the print_task(s).
Right now, the sock variable in the print_task() is undefined value on the print_task's stack, so you can't send() via undefined socket.