Hi All,
has anyone seen/fixed this before?
Im using the kinetis k60dn512 with MQX 4.1.1
If running in the debugger (codewarrior 10.6) I occasionally see that the ide break as if at a breakpoint and there is errors in the MQX errors tab:
in the 'MQX Errors' tab I see:
*Tasks:
Error: Unable to access task list
*Task Queues:
Task Queue address invalid 0x1ffff5fa8
and in the 'MQX Task Queues' tab in the task queues column:
Queue address invalid 0x1ffff5fa8
Doesnt appear to cause any runtime issues that ive noticed but sometihng isnt right.
Any ideas?
Hello Jonathan,
I tested using several MQX examples and I cann't reproduce this issue.
So maybe the installation is corrupted. Please try uninstalling MQX and installing it again.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Soledad,
Ive checksummed my copy of MQX and compared with a fresh install on another machine.
Nothing amiss except cproject and example make files being different so doesn't look like any corruption.
Also realised im on MQX 4.1.0 not 4.1.1.
I wouldnt expect you to find MQX throwing errors in mqx example code as then it would'nt be a very good example!
Is there a reference of what MQX errors might mean?
Thanks
Jon