Dear Sir/Madam,
I have our own Vybrid VF3x board a cash register. I have installed ARM-DS5, and MQX on windows7. I compiled and build all bsp and psp libraries as explained in " Getting Started with ARM® Development Studio 5 (DS-5™) with Freescale MQX™ RTOS" document, exported helloWorld2 project into my workspace, compiled, built, and now I can debug it with openSDA and DS-5 debugger.
I have a real time clock chip in my hardware. I want to integrate its SW into my helloworld2 project.
I am using I2C1 pins, how can I tell to MQX that I, it should prepare relevant pins accordingly? Is
MQX_FILE_PTR I2C_FILE=NULL;
I2C_FILE = fopen ("i2c1:", NULL);
enough?
There is an _i2c_init structure; How can I use it to define the I2C parameters, with FILE_PTR? could you please give me an example?
Best regards.
Mehmet Ali Ipim
已解决! 转到解答。
Hi,
You can modify the user_config.h file as follow:
#define BSPCFG_ENABLE_I2C1 1 //if you use Polled I2C
#define BSPCFG_ENABLE_II2C1 1 //if you use interrupt I2C
Then in the init_bsp.c, _bsp_enable_card will install I2C component.
Best Regards,
Susan
Hi Mehmet,
If you want to set the i2c baud rate ,for example 100KHZ, you can refer to the following code:
param = 100000; // baud rate 100KHZ
ioctl (fd, IO_IOCTL_I2C_SET_BAUD, ¶m);
In my opinion, IO_IOCTL_I2C_SET_BAUD is to tell the ioctl function to run the related code, in function _ki2c_polled_ioctl which is defined in mqx/source/io/i2c/polled/i2c_pol_ki2c.c:
case IO_IOCTL_I2C_SET_BAUD:
if (NULL == param_ptr)
{
result = I2C_ERROR_INVALID_PARAMETER;
}
else if (i2c_ptr->S & I2C_S_BUSY_MASK)
{
result = I2C_ERROR_DEVICE_BUSY;
}
else
{
i2c_ptr->F = _ki2c_set_baudrate( BSP_I2C_CLOCK, *param_ptr );
}
break;
Hope this could be useful!
Best Regards,
Susan
Hi Mehmet,
Please try using the C:\Freescale\Freescale_MQX_4_0_2_GA\mqx\examples\i2c project as reference to using I2C.
Susan is correct for enabling the BSP to pre-load the polled or interrupt driver for I2C but best to only enable one or the other and not both.
Regards,
David
Dear Susan/David,
Thank you for your helps. I have read the project and i2c.c file for example. for the baud rate
#define IO_IOCTL_I2C_SET_BAUD _IO(IO_TYPE_I2C,0x01)
id defined. What the value for this? for example is it 100KHz, 400kHz?
Thanks and best regards.
Mehmet
Hi,
You can modify the user_config.h file as follow:
#define BSPCFG_ENABLE_I2C1 1 //if you use Polled I2C
#define BSPCFG_ENABLE_II2C1 1 //if you use interrupt I2C
Then in the init_bsp.c, _bsp_enable_card will install I2C component.
Best Regards,
Susan