Solved! Go to Solution.
I found a solution!
If you use demos from mqx\demo you need do following:
To enable the TWR-SER RS232 interface change the BSP_DEFAULT_IO_CHANNEL configuration option to "ttyd:" in the mqx\source\bsp\twrk40x256\twrk40x256.h file.
If you use demos from KINETIS512_SC you need do following:
To enable the TWR-SER RS232 interface uncomment
#define SERIAL_CARD
and comment
//#define OSJTAG
in the KINETIS512_SC_1.4\src\platforms\k40_tower.h file.
Best regards.
The problem was solved =).
Best regards.
What is a solution?
I found a solution!
If you use demos from mqx\demo you need do following:
To enable the TWR-SER RS232 interface change the BSP_DEFAULT_IO_CHANNEL configuration option to "ttyd:" in the mqx\source\bsp\twrk40x256\twrk40x256.h file.
If you use demos from KINETIS512_SC you need do following:
To enable the TWR-SER RS232 interface uncomment
#define SERIAL_CARD
and comment
//#define OSJTAG
in the KINETIS512_SC_1.4\src\platforms\k40_tower.h file.
Best regards.