Hi Folks,
In the main process of my application, inside one function, I call another function which uses the tty(b) driver to send out an ASCIIZ string. When this function is called, the app crashes (and causes a segmentation fault on my PC which is running CW when I'm debugging - which is strange).
However, if the error condition which causes the upchuck during the tty write does not occur, execution continues normally - in fact, the tty ASCIIZ function is called later in the program to give a status and there are no issues.
I suspect that I have a stack issue in the main process - is there any way to confirm that this is what's happening?
Does anybody have any ideas why CW has the crash as well?
Thanx,
myke
解決済! 解決策の投稿を見る。
You may try to use the task aware debugging (TAD) in codewarrior. It shows you the stack memory and stack overflow situations.
You may try to use the task aware debugging (TAD) in codewarrior. It shows you the stack memory and stack overflow situations.
Hi Mark,
Thank you - that sounds like a good suggestion.
I increased the task's stack by 256 bytes and the problem has gone away.
I'm still curious as to why I had the problem with CW and the PC it is running on - anybody have any ideas?
myke