Greetings,
I have MQX 3.6.0 installed and I found in the site the MQX 3.6.2 update patch.
But it says it's from 3.6.1 to 3.6.2. Can I use it on 3.6.0 or should I first update to 3.6.1? But I can't find a 3.6.0->3.6.1 update file...
Hello,
You should be able to upgrade multiple ways...either the incremental approach you mention. Here is link to FSLMQX3/6/1 patch/
http://www.freescale.com/webapp/sps/site/overview.jsp?code=MQXSWDWARCH&tid=m32MQX
Or just download the entire FSLMQX3.6.2 installer:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MQX&tab=Design_Tools_Tab
Regards,
David
I just posted another thread about this, then found this thread, so I will move my post here!
It appears that the update.exe has an error, if you read the error message you get:
Quote:
Fresscale MQX 3.6 - InstallSheild Wizard
The Setup has detected older version of MQX.
You have to update to Freescale MQX version 3.6.2 before installing this patch
Must be 3.6.2 to install 3.6.2? My head hurts
Hi Carl,
I've notified our FSLMQX developers of the update patch issue.
In mean time try the install of the full FSLMQX3.6.2. I did this yesterday without issue...hope that is same for you.
Regards,
David
You are right there is bug in the FSLMQXOS_3_6_2_update.exe (differential update package). The bug appears in following scenario.
FSLMQXOS_3_6_1(full) -> FSLMQXOS_3_6_2_update.exe
The scenarios bellow should work fine:
FSLMQXOS_3_6_0 -> FSLMQXOS_3_6_2.exe (full)
FSLMQXOS_3_6_0 -> FSLMQXOS_3_6_2_update.exe
FSLMQXOS_3_6_0 -> FSLMQXOS_3_6_1.exe (full or update) -> FSLMQXOS_3_6_2_update.exe
FSLMQXOS_3_6_0 -> FSLMQXOS_3_6_1.exe (full or update) -> FSLMQXOS_3_6_2.exe (full)
FSLMQXOS_3_6_1 -> FSLMQXOS_3_6_2.exe (full)
FSLMQXOS_3_6_2.exe (full) stand alone
We are working on the solution. Fixed FSLMQXOS_3_6_2_update.exe should be available tomorrow.
Note - if you experienced unsuccessful installation using FSLMQXOS_3_6_2_update.exe then you have to use full install package (FSLMQXOS_3_6_2.exe) for installation. After installing update you must to run it again; select Modify and enable the features which are new in MQX 3.6.2 (TWR-K60, TWR-K40 BSPs and IAR extensions).
We are very sorry for inconvenience.
PetrL
Thanks David / Peter, intalling the complete install worked just fine. Thanks.
Hello,
MQX 3.6.2 refuse to install over 3.6.1, it always complains about it doesn't find previous release.