I try to run the demo web_hav, but I am not able to see the webpage
I am using
- a TWR-K60D100 Tower Modul
- code warrior 10.3 eva
- MQX 4.0
I import the project
#define DEMOCFG_ENABLE_WEBSERVER 1
#define DEMOCFG_ENABLE_RTCS 1
When I debugging I can see that in the procedure HVAC_initialize_networking()
- the ipcfg_bind_staticip is ok
- httpd_server_run(server) is ok
I have set the jumper as described in the user manual document.
When I checked the LAN connection in Window 7, I see correct IP address 169.254.3.3
but when I try to see the web page in the browser (firefox) 169.254.0.1 I get an error message.
Has somebody an idea what's going wrong. I try the whole day and could not find the reason.
There is another thing I don't understand.
As soon as I activate the shell, the other tasks are not running. I never reached the breakpoints in the other tasks.
解決済! 解決策の投稿を見る。
Dear Martin, thanks for your reply.
I have found the reason for my described problem. The IIS7 webserver was already started and used the same port as the hvac websever. After I had finished the service, the example works fine.
I'm looking into HVAC.h and I can see the ENET_IPADDR of the TWR board is set to 169.254.3.3.
Is this the confusion ? You should configure your PC to manual IP 169.254.0.1 and try to open 169.254.3.3 from firefox web browser.
Dear Martin, thanks for your reply.
I have found the reason for my described problem. The IIS7 webserver was already started and used the same port as the hvac websever. After I had finished the service, the example works fine.