I have a Codewarrior 10.3 project developed also using Processor Expert.
There is a possibility to make it run under MQX without the need to remake the project? it's possible to trasform this project in one or more MQX tasks?
Please, help me!
Thanks. Abele
Hi Abele,
if you have developed your project on Kinetis derivative which is supported by MQX than it is possible. You can export settings of PEx components in your baremetal application using
This is just simple workflow as I do not know any details about your application. Transfering baremetal code into RTOS is little bit tricky. The description above do not take care about application optimization and splitting baremetal superloop into tasks and using RTOS synchronization objects for better performance as this is application specific.
Regards Petr
Hi Petr
I have performed the first four steps as your list, but when I rebuild bsp project i find many errors (see image here attached)
Have you any further suggestion about?
Many thanks in advance.
Regards
Abele
From: petr.uhlir
Sent: Tuesday, April 23, 2013 10:35 AM
To: abele barbieri
Subject: Re: MQX Software Solutions - Porting project to MQX
Porting project to MQX
created by petr.uhlir in MQX Software Solutions - View the full discussion
Hi Petr
I made a few tests with Processor Expert included in BSP. I think I found an issue related to Logical Device Driver BitIO_LDD and BitsIO_LDD. If I added one of these component, PE generates the files .s and .h for the build, but when you build the BSP library it does not create the object referred, and then produces error.
I think that there is a trouble in CW10.3 using MQX and Processor Expert. I attach Codewarrior screenshot to best understand.
Reagrds
Abele
From: petr.uhlir
Sent: Friday, April 26, 2013 1:50 PM
To: abele barbieri
Subject: Re: MQX Software Solutions - Porting project to MQX
Porting project to MQX
created by petr.uhlir in MQX Software Solutions - View the full discussion
Sorry, I was wrong file ...
here right file
From: petr.uhlir
Sent: Friday, April 26, 2013 1:50 PM
To: abele barbieri
Subject: Re: MQX Software Solutions - Porting project to MQX
Porting project to MQX
created by petr.uhlir in MQX Software Solutions - View the full discussion