Pins of SPI1 on K60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pins of SPI1 on K60

Jump to solution
1,322 Views
tfrauenrath
Contributor III

Hi there,

in the datasheet of the K60 (9/2011) I see that SPI1 is connected to Pins

CS0 --> PTE4

CLK --> PTE2

SOUT --> PTE1

SIN --> PTE3

which are mentioned in "ALT2" configuration.

The example provided in C:\Freescale\Freescale MQX 3.8\mqx\examples\spi\uv4\twrk60n512 is functional in these pins when I activate SPI1 in user_config.h  (at least I can see activity with my scope on these pins)

How can I change SPI1 to these pins

CS0 --> PTB10

CLK --> PTB11

SOUT --> PTB16

SIN --> PTB17

which are also mentioned in "ALT2" configuration.

Tags (5)
1 Solution
990 Views
Martin_
NXP Employee
NXP Employee

Pin assignment is configured in BSP, for your twrk60n512 that is:
c:\Freescale\Freescale MQX 3.8\mqx\source\bsp\twrk60n512\init_gpio.c

In the _bsp_dspi_io_init(), you need to change:

case 1:
    /* Configure GPIOE for DSPI1 peripheral function     */
    pctl = (PORT_MemMapPtr)PORTE_BASE_PTR;

    pctl->PCR[1] = PORT_PCR_MUX(2);     /* DSPI1.SOUT   */
    pctl->PCR[2] = PORT_PCR_MUX(2);     /* DSPI1.SCK    */
    pctl->PCR[3] = PORT_PCR_MUX(2);     /* DSPI1.SIN    */
    pctl->PCR[4] = PORT_PCR_MUX(2);     /* DSPI1.PCS0   */

    /* Enable clock gate to DSPI1 module */
    sim->SCGC6 |= SIM_SCGC6_SPI1_MASK;
break;

to

case 1:
    /* Configure GPIOB for DSPI1 peripheral function     */
    pctl = (PORT_MemMapPtr)PORTB_BASE_PTR;

    pctl->PCR[16] = PORT_PCR_MUX(2);     /* DSPI1.SOUT   */
    pctl->PCR[11] = PORT_PCR_MUX(2);     /* DSPI1.SCK    */
    pctl->PCR[17] = PORT_PCR_MUX(2);     /* DSPI1.SIN    */
    pctl->PCR[10] = PORT_PCR_MUX(2);     /* DSPI1.PCS0   */

    /* Enable clock gate to DSPI1 module */
    sim->SCGC6 |= SIM_SCGC6_SPI1_MASK;
break;

And then make sure you disable or re-map other drivers that map onto those pins.

For example, electrodes for TSI are mapped to PORTB_PCR16 and PORTB_PCR17 in _bsp_tss_io_init() function.

View solution in original post

2 Replies
991 Views
Martin_
NXP Employee
NXP Employee

Pin assignment is configured in BSP, for your twrk60n512 that is:
c:\Freescale\Freescale MQX 3.8\mqx\source\bsp\twrk60n512\init_gpio.c

In the _bsp_dspi_io_init(), you need to change:

case 1:
    /* Configure GPIOE for DSPI1 peripheral function     */
    pctl = (PORT_MemMapPtr)PORTE_BASE_PTR;

    pctl->PCR[1] = PORT_PCR_MUX(2);     /* DSPI1.SOUT   */
    pctl->PCR[2] = PORT_PCR_MUX(2);     /* DSPI1.SCK    */
    pctl->PCR[3] = PORT_PCR_MUX(2);     /* DSPI1.SIN    */
    pctl->PCR[4] = PORT_PCR_MUX(2);     /* DSPI1.PCS0   */

    /* Enable clock gate to DSPI1 module */
    sim->SCGC6 |= SIM_SCGC6_SPI1_MASK;
break;

to

case 1:
    /* Configure GPIOB for DSPI1 peripheral function     */
    pctl = (PORT_MemMapPtr)PORTB_BASE_PTR;

    pctl->PCR[16] = PORT_PCR_MUX(2);     /* DSPI1.SOUT   */
    pctl->PCR[11] = PORT_PCR_MUX(2);     /* DSPI1.SCK    */
    pctl->PCR[17] = PORT_PCR_MUX(2);     /* DSPI1.SIN    */
    pctl->PCR[10] = PORT_PCR_MUX(2);     /* DSPI1.PCS0   */

    /* Enable clock gate to DSPI1 module */
    sim->SCGC6 |= SIM_SCGC6_SPI1_MASK;
break;

And then make sure you disable or re-map other drivers that map onto those pins.

For example, electrodes for TSI are mapped to PORTB_PCR16 and PORTB_PCR17 in _bsp_tss_io_init() function.

990 Views
carlos_neri
NXP Employee
NXP Employee

Tobias,

Both pin assignments are correct.

SPI1 (and other modules) signals are routed to different ports, this enables some flexibility when designing schematics for your application.

0 Kudos
Reply