NanoSSL, MQX 4.1, and K60D100 TWR - Will it work?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NanoSSL, MQX 4.1, and K60D100 TWR - Will it work?

526 次查看
chinniwhites
Contributor II

I need to send secure emails using the likes of gmail, yahoo, etc.  All documentation for NanoSSL is for MQX 3.7 using Coldfire processors.  Documentation also alludes to there being a a processor expert component for the NanoSSL but I dont understand how that happens if I am just adding some source and header files from NanoSSL into my project.

1) Will NanoSSL work with MQX 4.1 with Kinetis K60?

2) Is there any updated documentation that shows how to add NanoSSL to existing project

3) Further details on how it ties into Processor Expert

Any help would be much appreciated.

标记 (5)
0 项奖励
1 回复

281 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Unfortunately NanoSSL/NanoSSH patch for MQX doesn't support Kinetis platforms yet. It is only for MQX and ColdFire.

This work on Kinetis support is in progress. Availability date can't be estimated as there is 3rd party partner (Mocana) involved.

There is an open source CyaSSL alternative that works on Kinetis and MQX already.

Topics about memory footrpint of this software are on the internet, for example:

http://sourceforge.net/projects/yassl/forums/forum/439591/topic/3775747

NanoSSL / NanoSSH price list here:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=NANOSSH&nodeId=0152103F6BEC94EE8C&tab...

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=NANOSSL&nodeId=0152103F6BEC94EE8C&tab...

Hope this helps!

--------------------------------------------------------------------------------

this answer is for you, if it helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 项奖励