Porting MQX to i.MX6 - Cortex A9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Porting MQX to i.MX6 - Cortex A9

1,554件の閲覧回数
Rob_iMX6
Contributor II

Did anybody try it?

We intend to do it, using just one core of the i.MX6 and supporting SPI, I2C, USB (Device), Ethernet (100Mbit/RMII 50MHz) and EIM.

By using the Vybrid A5 as a starting point, this should be feasible.

Maybe someone has some comments on this? Any comments are more than welcome!

We are willing to share the ported code, if there is some interest.

Regards,

-Urs

タグ(1)
0 件の賞賛
返信
2 返答(返信)

922件の閲覧回数
RadekS
NXP Employee
NXP Employee

We are currently working on MQX port for i.MX6SX. It will be released in near feature as standalone MQX release.


Best Regards,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

922件の閲覧回数
RadekS
NXP Employee
NXP Employee

I would like to apologize. I forget mention that MQX port for i.MX6SX will be only for M4 core. A9 core will be not directly supported.

If you would like use MQX for A9 core, you can contact Freescale Professional Services:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_PROFESSIONAL

0 件の賞賛
返信