MQX Vybrid support

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

MQX Vybrid support

1,733件の閲覧回数
POSterminalPCI_
Contributor II

Dear Sir/Madam,

Hello,

Is MQX available for Vybrid processors?. If not when it will be available?

Is there ISO 7816 support for MQX?

Best regards.

Mehmet Ali Ipin

ラベル(1)
タグ(1)
5 返答(返信)

635件の閲覧回数
c0170
Senior Contributor III

Hello Mehmet Ali Ipin,

VYBRID processors are going to be supported in next MQX release which should be released in Q2 2013.

Regards,

MartinK

635件の閲覧回数
POSterminalPCI_
Contributor II

Dear Martin,

Thank you for your answer,

Is it for only Cortex M4 or, Cortex A5-specially VF3XX also supported?

Thanks and best regards.

0 件の賞賛

635件の閲覧回数
c0170
Senior Contributor III

Hello,

VF6XX will be supported in the MQX.

Regards,

MartinK

0 件の賞賛

635件の閲覧回数
JohnGoodman
Contributor I

So does that means MQX will support VF5XX that has a Cortex-A5 only?

0 件の賞賛

635件の閲覧回数
hongtranduc
Contributor II

To be more specific, the MQX is supported Cortex-M4 already, and Cortex-A5 will be supported in this year release.