I am not able to find MQX Tool in Code warrior 10.2 menu bar (Windows 7 OS )
How to enable MQX Tool in Code warrior 10.2.
I have already followed the procedure of code warrior extensions Readme file(install_cw10.2_plugin.bat) but still not able to view MQX Tool plugin in Code warrior 10.2
Please give stepby step procedure for this
Thanks
V.Gowrishankar
已解决! 转到解答。
hi VGS,
You have to run command line and actual directory must be set to MQX ROOT FOLDER/tools/codewarrior_extensions/CW MCU v10.2 so it recognizes bat file located there.
Run this command : install_cw10.2_plugin.bat "C:\Program Files\Freescale\CW MCU v10.2"
"C:\Program Files\Freescale\CW MCU v10.2" is location of installed CW 10.2 in my case. Replace it with your path.
Regards,
MartinK
Hi, I've done everything exactly as described here, and as described in the readme.txt file inside the codewarrior_extensions directory. Here is the output from running the batch file.
c:\Freescale\Freescale MQX 3.8\tools\codewarrior_extensions\CW MCU v10.2>install
_cw10.2_plugin.bat c:\Freescale\CW MCU v10.2
**** Installing CW10.2 Task Aware Debugging and New Project Wizard Plugins ***
**** It can take up to 60 seconds ***
**** Installing plug-ins for MQX 3.8 ****
The system cannot find the path specified.
**** Installing plug-ins for MQX - all versions ****
The system cannot find the path specified.
**** Installing CW10.2 Processor Expert MQX RTOS Adapter update ****
17 File(s) copied
**** Done ****
It is having trouble finding the path for CW 10.2, but I can assure you that I have it installed at "c:\Freescale\CW MCU v10.2". I'm running Windows 7 64 bit. Is it possible it doesn't like the spaces in the path? I think I saw another post discussing that, but it might only pertain to an older version of CW.
It did install the CW 10.2 RTOS Adapter Update, but it looks like it put it in a whole other directory "C:\Freescale\CW"...this makes me even more suspicious about the spaces in the path. Anybody have any insight?
hello rgardner,
The question you have described I have faced before.
You must login you PC by administrator and then reinstall CW 10.2 and MQX 3.8 ; Last, follow the readme.txt file inside the codewarrior_extensions directory.
best wishs
kris
Hi rgardner,
I checked your output, you have to wrap up the path into quotes "c:\..your path". That's why the output was no path specified. It processed the input only until a first space character : c:\Freescale\CW not c:\Freescale\CW MCU v10.2
Regards,
MartinK
I had to do the following in order to get the MQX new project wizard to appear within the CodeWarrior menu. The various readme.txt instructions are not clear.
If you run the batch file without specifying the command line parameter then it displays a help message explaining that you have to specify the CodeWarrior installation folder on the command line. This is why you need to run the batch file from an DOS prompt instead of simply opening it from Windows Explorer.
Thanks for your comment!
You are right that Step 1 is not necessary.
Here is what I did:
1. Open a DOS prompt and CD to "[MQX_INSTALL_DIR]\tools\codewarrior_extensions\CW MCU v10.2"
2. Enter the command "install_cw10.2_plugin.bat [CW_INSTALL_DIR]"
hi VGS,
You have to run command line and actual directory must be set to MQX ROOT FOLDER/tools/codewarrior_extensions/CW MCU v10.2 so it recognizes bat file located there.
Run this command : install_cw10.2_plugin.bat "C:\Program Files\Freescale\CW MCU v10.2"
"C:\Program Files\Freescale\CW MCU v10.2" is location of installed CW 10.2 in my case. Replace it with your path.
Regards,
MartinK