MK20DX128VFM5不工作

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK20DX128VFM5不工作

4,598件の閲覧回数
xiebaokui
Contributor II

买了几个MK20DX128VFM5芯片,电路图见附件

将USB插入电脑,没有任何反应,识别不了USB口,

测试如下:

TP3003(VBAT): 0.659V

TP3002(EXTAL32):0V

TP3001(XTAL):0V

TP3012(ADC0):3.3V

GPIO20 GPIO19:0.017V

8MHz 晶振未起震

タグ(1)
7 返答(返信)

4,081件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

VBAT provides power to 32KHz oscillator and RTC modules.

I would recommend customer to refer TWR-K20D50M board schematics about power and SWD debugger interface circuit.

The system oscillator and 32KHz oscillator need software to enable internally.

Please download and refer K20 50MHz bare-metal software here.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

4,080件の閲覧回数
xiebaokui
Contributor II

你好,我参照TWRK20D50M_SCH.PDF文档操作,给VBAT供电3V3,32.768KHZ晶振也接在了EXTAL32和XTAL引脚上,供电后依然无法工作。

有尝试过

按下并保持SW3001(RESETB_TGT3V3)开关,将USB插入电脑,我的电脑一直出现不了mass storage,无法更新MK20固件

附件为完整的SCH文件,请帮忙看下问题出在哪里?谢谢

0 件の賞賛

4,080件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

First of all, sorry for the later reply.

I think you want to make MK20 works as on board OpenSDA debugger tool. Right?

If yes, I would recommend customer to check here for OpenSDA debugger tool resource.

The FRDM-K28F is using the latest OpenSDA v2.2 , which provided OpenSDA and bootloader firmware.

pastedImage_1.png

The OpenSDA circuit should refer FRDM-K28F board schematics .

Please let me know if there still with any updated query. Thanks.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,080件の閲覧回数
haoxue1027
Contributor IV

hi,hui_ma

If i want to make MK20 works as on board OpenSDA debugger tool on the DEVKITMPC5744P.

where to find OpenSDA debugger tool resource.

pastedImage_1.png

there is not an option for DEVKITMPC5744P.

 best regards

hao

0 件の賞賛

4,080件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Hao,

Could you post your question at MPC5xxx sub-forum

My colleague could help with that thread. Thanks.

best regards,

Mike

4,080件の閲覧回数
haoxue1027
Contributor IV

hi  Hui_Ma

thanks for your suggestion.

best regards,

hao

0 件の賞賛

4,081件の閲覧回数
xiebaokui
Contributor II

你好,我参照TWRK20D50M_SCH.PDF文档操作,给VBAT供电3V3,32.768KHZ晶振也接在了EXTAL32和XTAL引脚上,供电后依然无法工作。

有尝试过如下:

按下并保持SW3001(RESETB_TGT3V3)开关,将USB插入电脑,我的电脑一直出现不了mass storage,无法更新MK20固件

附件为完整的SCH文件,请帮忙看下问题出在哪里?谢谢

0 件の賞賛