Hi All,
I was wondering if the bsp, psp for K60N512 is compatible for K60F150.
If not, how could I migrate it from K60N512 to K60F150 or how could I create a new one for K60F150?
Thank you.
-Daniel
解決済! 解決策の投稿を見る。
Hi Daniel,
I believe you should be able to use the K70 BSP without issues. The K70 also runs at 150 MHz and that makes them compatible in the MQX BSP.
Good luck!
Best Regards,
Garabo
Hi Daniel,
I believe you should be able to use the K70 BSP without issues. The K70 also runs at 150 MHz and that makes them compatible in the MQX BSP.
Good luck!
Best Regards,
Garabo
To add to what Garabo stated, the K70 BSP clocks the core at 120MHz generated from the 50MHz external oscillator, as shown in the MQX Getting Started guide. But if a BSP is cloned and ported to your K60F150 device, the clock configuration in the BSP can be modified to clock the core at 150MHz. An easy way to change the clock configuration in the BSP like this is to use Processor Expert, and this is documented in the file installed with MQX at
<MQX Installation Directory>\doc\tools\cw\Howto_SetupKinetisClock_UsingPE.pdf
Also, another good BSP that could be used to port to a K60F150 device is the twrk60f120m BSP. This BSP also clocks the core at 120MHz and can be updated to 150MHz. But it could require less changes. If you were using a K60F device with external DRAM, the K70 BSP would be a better fit to start with since it supports DDR2. A K60F without DRAM is probably closer to the twrk60f120m BSP.
Hi Derek,
After I reading the manual for porting the BSP, I get confused.
It seems I need to change lots of the low-level drivers for the hardware parts. Am I correct?
Thanks.
-Daniel
The vast majority of the files you need to change start with init_ and can be found in the \mqx\source\bsp\<board_name> directories. The MQX drivers are written to be as agnostic to the hardware as possible.
init_gpio.c, ini_hw.c & board_name.h are going to be the most time consuming.
It is a time consuming process (because of the number of details) but not particularly hard. However there is reason BSP engineers get paid more than software programmers...
Hi Garabo,
Thank you.
If I want to create a new one, how should I do that?
-Daniel
Hi,
Also we have the clone wizard option. You can find the documentation in the MQX 4.0.1 version in the path:
C:\Freescale\Freescale_MQX_4_0\doc\tools\MQX_BSP_Cloning_Wizard_Getting_Started.pdf
The tool is located in the path:
C:\Freescale\Freescale_MQX_4_0\tools\BSPCloningWizard
Hope this helps.
Garabo