Hi,
I am new to K70 and freertos. I am not sure if freescale provides library files for freertos or i would have to erite my own library for peripherals. even like GPIO and UART. Any help will be highly appreciated.
Thanks
Hello,
Unfortunately we do not provide FreeRTOS and IAR support, however you can check the below links as reference.
http://www.freertos.org/FreeRTOS-for-K60-Cortex-M4-with-web-server.html
In addition we suggest you to use MQX, Freescale MQX™ RTOS is a full-featured complimentary real-time operating system including the MQX™ Kernel, TCP/IP stack (RTCS), embedded MS-DOS file system (MFS), USB host/device stack, and more. The MQX™ multitasking kernel provides pre-emptive scheduling, fast interrupt response, extensive inter-process communication and synchronization facilities. MQX RTOS includes its own peripheral drivers.
You can download it from the below link:
Freescale MQX™ Software Solutions|Freescale
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------