Does MQX rtos have graphics library included with it ? Is MQX RTOS certified for medical devices? I want to Design class II medical device with freescale chips.
Hello,
There are two options for graphics library as “add-on software for Freescale MQX
http://www.freescale.com/webapp/sps/site/overview.jsp?code=THIRDPARTY
1. Swell Software provides Graphical User Interface (GUI) Solutions for Embedded Devices. Swell's PEG Pro, PEG+ and C/PEG product offering includes a Graphical User Interface (GUI) library for embedded development that works tightly with real-time operating systems.
Available from Swell Software PEG Product Line
2. The complimentary Freescale embedded graphical user interface (eGUI) allows single chip microcontroller (MCU) systems to implement a graphical user interface and drive the latest generation of color graphics LCD panels with integrated display RAM and simple serial peripheral interface (SPI) or parallel bus interface.
Available from Freescale EGUI
For those who must follow a formal certification process, the MQX RTOS platform has a record of past certifications in medical specifications (CFR 820.30 Part 21, IEC 60601-1) and the aerospace requirements listed under DO-178b. Safety critical applications based on MQX RTOS include eye surgery equipment, drug injection equipment, radiation dose monitoring equipment, aircraft braking systems and aircraft navigation equipment.
However we don't have access to any certification certificates, or a letter that certifies such credentials. We don’t have any document because our customers are the once that follow those processes. We don’t certify Freescale MQX on any certification. We cannot share any document because we don’t have them. They are owned by other customers and this information cannot be share with us so we cannot share. The alternative is to go to a company that specializes in such accreditation.
Our 3rd party partner Embedded Access might have more information for you in this regard.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Shaikh
Please check the following link for Graphics Library.
PEG Graphics Software|Freescale
Regards
Daniel