Freescale MQX 4.0.1 Released!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Freescale MQX 4.0.1 Released!

2,311 次查看
macl
Senior Contributor I

Freescale MQX RTOS 4.0.1 is now available!

New architecture supported in MQX 4.0.1

ARM Cortex™-A5  on Freescale Vybrid F-Series MCUs

New board support packages added in MQX 4.0.1

BSPs for Vybrid F-Series Dual Core MCUs

    • MQX 4.0.1 for TWR-VF65GS10_A5  (Vybrid Tower Module Cortex™-A5)
    • MQX 4.0.1 for TWR-VF65GS10_M4  (Vybrid Tower Module Cortex™-M4)

New Features and Updates in MQX 4.0.1

Enhanced Tools Support

New Hardware Timer driver

Multicore Communication (MCC) for inter-core (OS) communication (MQX-to-MQX or MQX-to-Linux)

Improved Internet Protocol version 6 (IPv6) Support - Available as Add-on

Enhanced BSP cloning wizard

Bug Fixes

   


标记 (3)
6 回复数

973 次查看
kubiznak_petr
Contributor V

Hi macl,

I've downloaded MQX 4.0.1 from the official site (Freescale MQX™ Software Solutions Product Summary Page) but the installer does only one thing - see the image.

4428_4428.png

Any idea what's wrong? Thanks.

Btw few days ago I installed MQX 4.0.1 Beta 3 (from Compass) successfully but the IAR build failed.

0 项奖励
回复

973 次查看
kubiznak_petr
Contributor V

The problem was in a broken download - for an unknown reason, instead of ~180 MB, my download finished at 19.6 MB. Tried repetitively with the same result, then tried from another computer with success. Don't understand what was wrong but that wasn't the first time that happened in our company - might be something wrong on the Freescale's servers?

Anyway, I got it installed and built successfully, everything ok now.

973 次查看
silodiq
Contributor I

Can download it now? We have encounter problem in lower power consumption testing, "can't wake up from lls mode ",we use  10M crystal, MK60FN1M0VMD12 ,maybe this version have fixed it?

0 项奖励
回复

973 次查看
c0170
Senior Contributor III

Hello silodiq,

yes, you can download it, just follow the first link provided in macl's post !

If you have problem with low power, test it with 4.0.1 , but I guess problem will be somewhere else. Create a new post if it's still relevant :smileywink:

Regards,

c0170

0 项奖励
回复

973 次查看
dspNeil
Contributor III

The link doesn't work outside of Freescale. I think this is what you meant: Freescale MQX™ Software Solutions Product Summary Page

0 项奖励
回复

973 次查看
silodiq
Contributor I

Hi Martin,

I have tried ,but can't download it,please check. Could you present Bug Fixes for detailedly?

Thanks & Best Regards.

0 项奖励
回复