Free Bare Metal/ No RTOS USB Stacks & Medical Connectivity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Free Bare Metal/ No RTOS USB Stacks & Medical Connectivity

2,051 Views
rav
Contributor III
No RTOS/Bare Metal USB Stacks
  • Reduced footprint available for MCUs down to 16 KBytes Flash and 512 Bytes SRAM
  • HID, MSD, CDC, Audio and PHDC USB.org standard classes are supported
  • Wide support within Freescale USB portfolio
  • Complimentary while using Freescale products
  • Code examples and documentation available
  • Guidelines to comply with recognized industry standard, such as Continua
  • Compatible with PHDC testing environment - development time is saved
  • MQX RTOS compatible

Click here to download  Support Kinetis End of March

 

Medical Connectivity Library 

The increased use of electronic devices in the medical domain has created a need for the development of a common protocol for data interchange between various devices. This problem is addressed by the IEEE-11073 Part 20601 (Optimized Exchange) specification. The Freescale Medical Connectivity Library is based on this specification and follows the Continua Health Alliance design guidelines for implementation.

 

Click here to download

 

Freescale_Medical_Library_v1.4_for_MQX_v3.7.exe  => End of March

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,479 Views
NoeSerres
Contributor II

Hi,

Can you update this post when Kinetis support is released?

End of march... it should be any minute now! :smileywink:

Thank you.

0 Kudos
Reply