I recently downloaded the MQX 4.0 release, and the release notes refer to availability of a flash translation layer (FTL) in the new version. The release notes say that this is available as a separate package. I haven't been able to locate it on freescale's website. Any idea when it is planned for release?
已解决! 转到解答。
Hello all,
if you haven't noticed, macl published new post with link to download NAND Flash file system, please check out the link:
NAND Flash File System patch for Freescale MQX™ RTOS 4.0.0
Regards,
MartinK
Hi V.K.,
MQX has a flash driver called FlashX that is used to access the on-chip flash for the various supported MCU's.
You can look at example:
C:\Freescale\Freescale_MQX_4_0\mqx\examples\flashx
You can look at the driver source code:
C:\Freescale\Freescale_MQX_4_0\mqx\source\io\flashx\freescale
Or download the baremetal Flash Drivers from web:
C90TFS_FLASH_DRIVER: TFS Flash Driver Software for Kinetis and ColdFire+ Microcontrollers.
Size (K): 9687 Format: exe Rev #: 0.3.3 Modified: 10/17/2012
Hope this helps.
Regards,
David
Hello all,
if you haven't noticed, macl published new post with link to download NAND Flash file system, please check out the link:
NAND Flash File System patch for Freescale MQX™ RTOS 4.0.0
Regards,
MartinK