When I load the TWR-K60N512_Quick_Start_Demo project, I get the following error
Tue Mar 01 14:45:47 2011: Fatal error: P&E Connection layer supports only Cortex M3/M4 devices. Session aborted!
- then when I try to make the project I get many errors ("cannot find file") and the project does not build. The MQX librarires built fine. I am using IAR Embedded workbench IDE 6.10. It seems like the project is not pulling in the libraries correctly, but I do not also understand the original error message.
any help