Hello
I'm working with "FFS" MQX 4.0 and K70.
Until today I was able to test with a driver "FFS" for MQX 3.81.
Now I have a problem.
I have developed code and prototypes with MQX 3.81 and "FFS".
Now bringing the code in MQX 4.0, I noticed that the formatting of fat NAND Flash is not compatible with the new driver MQX 4.0.
How do I import the data or at least make compatible the two formats?
Maurizio
there are two configuration #defines for the ffs:
in MQX 3.8.1 nandflash_wl.h after installation they are
#define NANDFLASH_1ST_DATA_DRIVE_SIZE_IN_BLOCK 90
#define NANDFLASH_1ST_DATA_DRIVE_START_BLOCK 10
in MQX 4.0 nandflash_wl_ffs.h they are
#define NANDFLASH_1ST_DATA_DRIVE_SIZE_IN_BLOCK 90
#define NANDFLASH_1ST_DATA_DRIVE_START_BLOCK 110
Have you tried to configure MQX 4.0 ffs to match MQX 3.8.1 ffs in these two values ?
I tried but it does not read MQX 4.0 formatting done with the MQX 3.81.
seems that uses two kinds of different formats.
Maurizio