Does MQX 4.0.2 CDC virtual_com run on the TWR-K20D50M?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does MQX 4.0.2 CDC virtual_com run on the TWR-K20D50M?

跳至解决方案
578 次查看
markgreggory
Contributor II

Does MQX 4.0.2 CDC virtual_com run on the TWR-K20D50M? There a project for the TWR-K21d50m in the CW10 folder that I loaded and changed the linker\debug settings to the TWR-k20d50. It compiles and runs but when I plug in the VCP USB cable into a windows machine nothing happens. TWR-k2050d jumpers are in the default setting.

Thanks,

Mark

标签 (1)
标记 (4)
0 项奖励
1 解答
435 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

can you please use C:\Freescale\Freescale_MQX_4_0\usb\device\examples\cdc\virtual_com\cw10\cdc_vcom_twrk20d72m .

在原帖中查看解决方案

0 项奖励
2 回复数
436 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

can you please use C:\Freescale\Freescale_MQX_4_0\usb\device\examples\cdc\virtual_com\cw10\cdc_vcom_twrk20d72m .

0 项奖励
435 次查看
markgreggory
Contributor II

Thank you ZhangJennie.

It worked, tight on RAM, but it worked. One problem though. I can't load the CDC drivers on Windows 8. They are not digitally signed. :smileysad:

Mark

0 项奖励