Does MQX 4.0.2 CDC virtual_com run on the TWR-K20D50M?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does MQX 4.0.2 CDC virtual_com run on the TWR-K20D50M?

ソリューションへジャンプ
1,352件の閲覧回数
markgreggory
Contributor II

Does MQX 4.0.2 CDC virtual_com run on the TWR-K20D50M? There a project for the TWR-K21d50m in the CW10 folder that I loaded and changed the linker\debug settings to the TWR-k20d50. It compiles and runs but when I plug in the VCP USB cable into a windows machine nothing happens. TWR-k2050d jumpers are in the default setting.

Thanks,

Mark

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,209件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

can you please use C:\Freescale\Freescale_MQX_4_0\usb\device\examples\cdc\virtual_com\cw10\cdc_vcom_twrk20d72m .

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,210件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

can you please use C:\Freescale\Freescale_MQX_4_0\usb\device\examples\cdc\virtual_com\cw10\cdc_vcom_twrk20d72m .

0 件の賞賛
返信
1,209件の閲覧回数
markgreggory
Contributor II

Thank you ZhangJennie.

It worked, tight on RAM, but it worked. One problem though. I can't load the CDC drivers on Windows 8. They are not digitally signed. :smileysad:

Mark

0 件の賞賛
返信