DNS SERVER

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DNS SERVER

1,557 次查看
thippeswamyj
Contributor I

Hello all,

I'm  using MQX 4.1. I want to use   www.dnsserver.com instead of an  IP address .  (ip is 192.168.1.202 --> 0xC0A801CA).

I define DNS parameters under source/if/dnshost.c the following way:

1. i enabled DNS

2.char DNS_Local_network_name[] = "arc.com.";

char DNS_Local_server_name[] = "DnsServer";

DNS_SLIST_STRUCT DNS_Local_server_list[] =

   {{DNS_Local_server_name, 0, 0xC0A801CA, 0, 0, 0, 0,

     0, DNS_A, DNS_IN }};

3.Then I call DNS_init() in my code.

actually the  dns task is created  but i am putting  www.DnsServer.com in chrome browser  but web page is not opening .it is opening

only for ip adress.

any one  can guide me, any other modification or any other function has to be add.

Regards

thippeswamy

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

1,092 次查看
vallinaths
Contributor II

Hi swamy ,

   it does not work that way DNS is feature used to identify  the IP address by name , so we need to put the DNS server IP available in the network or the ISP provided IP address . in the DNS server you need have entry of the MQX device so it can identify the ip address and provide the hostname

0 项奖励
回复

1,092 次查看
soledad
NXP Employee
NXP Employee

Hi Thippeswamy J,

Please check the below thread:

DNS under MQX 4.1

I hope this helps, have a nice day!
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,092 次查看
frandelgado
Contributor I

I have a problem with dns, dns did not work. I have the k60 module with MQX 3.7 operating system. The dns's introduce this:

while (DNS_init ()! = RTCS_OK)

{

_time_delay (1000);

}

strcpy (string, "google.com.");

host = gethostbyname (string);

while (host == NULL)

{

if (host! = NULL) {

name = host-> h_name;

alias1 = host-> h_aliases [0];

name2 = host-> h_aliases [1];

type = host-> h_addrtype;

length = host-> h_length;

ipDNS = * (uint_32_ptr) host-> h_addr_list [0];

}

host = gethostbyname (string);

}

When initializing the ethernet I have to call the function ipcg_add_dns?

  ipcfg_init_device (DEMOCFG_DEFAULT_DEVICE, address);

_ip_address DNS_server_ipaddr;

    DNS_server_ipaddr = inet_addr ("8.8.8.8");

    if (ipcfg_add_dns_ip (DEMOCFG_DEFAULT_DEVICE, DNS_server_ipaddr) == TRUE)

     {

     printf ("DNS added ok");

     } else {

     printf ("DNS added NOT ok");

     }

In addition to the file dnshosts.c must configure something?

thank you

0 项奖励
回复