Changing from K60 to K64

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Changing from K60 to K64

541 次查看
jesperevertsson
Contributor IV

Hi, for the past few years we've been using the MK60FX512 CPU. Now we are running out of RAM in our larger products and are looking to upgrade to a MK64FX512. We have a custom BSP, which is based on the K60F120M BSP, and now I'm wondering what's the easiest way going forward. Is it possible to just change the MQX_CPU define in "user_config.h" from our current K60 to the K64. That would be really easy for us since we've made some changes in some mqx source files for our current BSP. Or is it better to make a new BSP that is cloned from the K64F120M BSP?

标记 (3)
0 项奖励
1 回复

404 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Jesper:

 

I think it is not possible to just change the MQX_CPU define in “user_config.h” from your current K60 to the K64.  Because there are some differences between them. You need to do some migration work.

There are two BSP porting guide under MQX documentation folder. You can use that as a starting point to port custom code to K64.

C:\Freescale\Freescale_MQX_4_2\doc\mqx\MQX_BSP_Porting_Example_User_Guide.pdf

C:\Freescale\Freescale_MQX_4_2\doc\mqx\MQX_BSP_Porting_Guide.pdf

 

 

Since K64 is supported in MQX 4.2, I think it’s better to make a new BSP that is cloned from the K64F120M, and add your custom code into this BSP.

 

Regards

Daniel

0 项奖励