Can't find sh_snmpsrv.c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't find sh_snmpsrv.c

551 Views
jesperevertsson
Contributor IV

I've been trying to implement SNMP in one of my applications and in the chapter on SNMP in the Freescale MQX™ RTOS RTCS User's Guide (IPv4 and IPv6) it says:

"Complete example code with whole MIB tree can be found in file sh_snmpsrv.c in folder %MQX_PATH%\nshell\source\rtcs". First of all I dont have a folder named "nshell" even though I suspect this is a typing error since I do have a folder named "shell". But I still don't have the file "sh_snmpsrv.c" in eihter MQX 420 or 411.

Labels (1)
Tags (2)
0 Kudos
3 Replies

436 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

Thank you for reporting this, I think there is a typing error.  I think this file is in the following folder

In KSDK 1.2 , is

C:\Freescale\KSDK_1.2.0\rtos\mqx\nshell\source\rtcs\

or In MQX 4.2 , is

C:\Freescale\Freescale_MQX_4_2\shell\source\rtcs

0 Kudos

436 Views
jesperevertsson
Contributor IV

Yes, but I've looked in C:\Freescale\Freescale_MQX_4_2\shell\source\rtcs as well and it isn't there either. In fact I've searched for the file name in the entire MQX folder and the file doesn't exist.

0 Kudos

436 Views
danielchen
NXP TechSupport
NXP TechSupport

This is a document typo, I have create an internal ticket to developers. Thank you again.

Regards

Danile

0 Kudos