I've been trying to implement SNMP in one of my applications and in the chapter on SNMP in the Freescale MQX™ RTOS RTCS User's Guide (IPv4 and IPv6) it says:
"Complete example code with whole MIB tree can be found in file sh_snmpsrv.c in folder %MQX_PATH%\nshell\source\rtcs". First of all I dont have a folder named "nshell" even though I suspect this is a typing error since I do have a folder named "shell". But I still don't have the file "sh_snmpsrv.c" in eihter MQX 420 or 411.
Hi
Thank you for reporting this, I think there is a typing error. I think this file is in the following folder
In KSDK 1.2 , is
C:\Freescale\KSDK_1.2.0\rtos\mqx\nshell\source\rtcs\
or In MQX 4.2 , is
C:\Freescale\Freescale_MQX_4_2\shell\source\rtcs
Yes, but I've looked in C:\Freescale\Freescale_MQX_4_2\shell\source\rtcs as well and it isn't there either. In fact I've searched for the file name in the entire MQX folder and the file doesn't exist.