Can someone tell me if ADC MUX runtime is supported in TWRK60F120M? I checked through the BSP files, and found that the muxsel parameter within the ADC structure (defined in adc_kadc_prv.h) is only used once in the _adc_hw_channel_init() function of the adc_kadc.c file, to select either channel A or B during hardware initialisation.
I am expecting to see a runtime function to alternate between channel A and B, i.e. when the value of A channel is read, it switches to B channel for the next conversion, and vice versa. However I don't see any such function in the BSP.
Please tell me if this is the case, as I need to be sure that I can use ADC0_SE7A and ADC0_SE7B at the same time.
已解决! 转到解答。
Hi Keith,
If you can share just the small portion without compromising your customer that would be great. Since MQX is free and the community really is setup to help one another the more we share the better for all.
There is a great appnote that might also be helpful to you and others.
AN4590 Using DMA to Emulate ADC Flexible Scan Mode on Kinetis K Series
A great search tool for appnotes, docs, example code for appnotes is:
http://www.freescale.com/infocenter/index.jsp
Just enter keyword in search box.
The AN4590 is pretty new and not certain why it is not found but I'll pass that onto the web folk.
Regards,
David
Regards,
David
Hi Keith,
If you can share just the small portion without compromising your customer that would be great. Since MQX is free and the community really is setup to help one another the more we share the better for all.
There is a great appnote that might also be helpful to you and others.
AN4590 Using DMA to Emulate ADC Flexible Scan Mode on Kinetis K Series
A great search tool for appnotes, docs, example code for appnotes is:
http://www.freescale.com/infocenter/index.jsp
Just enter keyword in search box.
The AN4590 is pretty new and not certain why it is not found but I'll pass that onto the web folk.
Regards,
David
Regards,
David