Is there anyway to initialize the ethernet/mac interface in MQX RTCS such that the PHY will force/advertise 100M only?
已解决! 转到解答。
Turns out that the mqx/bsp project includes code/a driver to init/control a ksz8041 which does not include writing to the correct registers to only negotiate 100M for a different PHY...
Hello Matti,
Please check the Radek's answer in the next thread and let me know if this helps.
10Mbps with LAN8720 and K70 - Communication wit... | NXP Community
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Sol,
Thanks, but the thread you linked seems to discuss periodically checking link status/speed in order to re-initialize the enet module to support adapting to different speeds/duplex when the ethernet connection is unplugged and re-connected to different switches/hubs during runtime. It didn't really help.
I need to set my PHY to only advertise 100M. It looks like changing “Auto-negotiation” to “Full_Duplex_100M” in the ENET_default_params struct in init_enet.c (for me it is located at mqx\source\bsp\myProject\init_enet.c, but may be different for others depending on how you setup a project) should solve my issue. However, I have made the change and my PHY still auto-negotiates...
Any other ideas?
Matti
Hello Matti,
Yes you are right, you need to change this setting in the ENET_default_params[] structure which is located in the file init_enet.c. In that structure change the second element from "Auto_Negotiate" to "Half_Duplex_10M" or "Full_Duplex_10M", "Half_Duplex_100M" or "Full_Duplex_100M". After these changes you need to Rebuild the BSP, PSP and RTCS libraries.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------