I got a example project from the support. There are some code which I don't know the function of the code in the project. The code is below.
# tbs_main_asm.s - Time Base example
# Rev 1 Aug 27 2004 S Mihalik
# Copyright Freescale Semiconductor, Inc 2004 All rights reserved.
.globl tbs_main_asm
.text
tbs_main_asm:
# INITIALIZE TIME BASE=0
e_li r4, 0 # Load immediate data of 0 to r4
mttbu r4 # Move r4 to TBU
mttbl r4 # Move r4 to TBL
# ENABLE TIME BASE
mfhid0 r5 # Move from spr HID0 to r5 (copies HID0)
e_li r4, 0x4000 # Load immed. data of 0x4000 to r4
or r5, r4, r5 # OR r4 (0x0000 4000) with r4 (HID0 value)
mthid0 r5 # Move result to HID0
# EXECUTE SOME CODE
e_nop
e_nop
e_nop
e_nop
# RECORD TBL
mftbl r5 # Move TBL to r5 to store TBL value
e_li r4, 0
e_li r5, 0
mtmsr r4
mfmsr r4
wrteei 1
mfmsr r5
se_blr # (Set a breakpoint here and read r5)
Solved! Go to Solution.
Hi,
the functionality of this code is comprehensibly described in the code comments.
First stage initialize registers TBU and TBL to value 0. Second stage writes 1 to TBEN bit. This enables Time Base (counter implemented in core). Then four nop instructions are executed and value in TBL register is copied to the register R5.
At last R4 and R5 are set to 0, MSR register is set to 0 and wrteei enables interrupts. Last instruction jumps to the address which is in LR register.
Regards,
Martin
Hi,
the functionality of this code is comprehensibly described in the code comments.
First stage initialize registers TBU and TBL to value 0. Second stage writes 1 to TBEN bit. This enables Time Base (counter implemented in core). Then four nop instructions are executed and value in TBL register is copied to the register R5.
At last R4 and R5 are set to 0, MSR register is set to 0 and wrteei enables interrupts. Last instruction jumps to the address which is in LR register.
Regards,
Martin
Thank you very much for your reply. I also want to know the function of this code , what kind of role it can achieve? I can't find any information from the reference manual of MPC5644A. Could you give me some reference documents ? Thank you very much again!
Hi,
in general it can be used for example for time measuring. In fact Time Base is very precise counter which is implemented in the core. In your case I am not able to tell you why is this code used in your project because I do not have it.
If you want some information about time base, try to look at the core reference manual.
http://cache.freescale.com/files/32bit/doc/ref_manual/e200z4RM.pdf?fsrch=1&sr=1&pageNum=1
Regards,
Martin