question about MPC5744p Flex_PWM output trigger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

question about MPC5744p Flex_PWM output trigger

2,539 次查看
fyw
Contributor IV

148951_148951.pngoutTrig.png

 

 

VAL0, VAL2, and VAL4 are used to generate OUT_TRIG0 and VAL1, VAL3, and VAL5 are used to generate OUT_TRIG1.  what does that mean?

 

As i understand,

Sub0_VAL2 will generate OUT_TRIG0_0 riseEdge(I1RE), Sub0_VAL3 will generate OUT_TRIG0_0 fallEdge(I1FE).

Sub0_VAL4 will generate OUT_TRIG1_0 riseEdge(I5RE), Sub0_VAL5 will generate OUT_TRIG1_0 fallEdge(I5FE),

 

Sub1_VAL2 will generate OUT_TRIG0_1 riseEdge(I2RE), Sub0_VAL3 will generate OUT_TRIG0_1 fallEdge(I2FE).

Sub1_VAL4 will generate OUT_TRIG1_1 riseEdge(I6RE), Sub0_VAL5 will generate OUT_TRIG1_1 fallEdge(I6FE),

 

Sub0_VAL0 will generate PWMX0 riseEdge(I9RE), Sub0_VAL1 will generate PWMX0 fallEdge(I9FE).

Sub1_VAL0 will generate PWMX1 riseEdge(I10RE), Sub0_VAL1 will generate PWMX0 fallEdge(I10FE).

 

Do i understand correct?  thank you very much!

标签 (1)
12 回复数

2,063 次查看
fyw
Contributor IV

thank you for Petr & Yanna!

0 项奖励
回复

2,063 次查看
yanna
Contributor IV

Hi,

I hope this figure could help you.

pastedImage_1.png

Yanna

0 项奖励
回复

2,062 次查看
PetrS
NXP TechSupport
NXP TechSupport

Yanna,

you are not correct. Here is a graphic explanation how OUT_TRIGx_y signals are generated. Here submodule's 0 OUT_TRIG0_0/OUT_TRIG0_1 signals are assumed and SUB0.TCTRL = 0x3F (all compare registers generate trigger pulse).

pastedImage_0.png

Petr

2,062 次查看
fyw
Contributor IV

Petr  thank you very much!

i still have 4 questions:

Q1: if i chose pwmx0 as the ctu tgsisr source(I9RE or I9FE =1), when does the signal pwmx0 happen(val0--->  riseEdge & fallEdge?)?  can you graphic for me? thank you very much!

Q2: if i want to use out_trig0_0 as the source,  according to your graphic, val0/2/4 will all generate out_trig0_0, but i only want to use val2 generate the signal. So do i need to set a special value to val0/4  in order to avoid generate out_trig0_0 signal?

Q3: if i want to use out_trig1_0 as the source,  according to your graphic, val1/3/5 will all generate out_trig1_0, but i only want to generate one pulse in a pwm period. So i no choice except for val1(val1 determins the period), is that correect?

Q4: if i set val0=val2=val4(or val1=val3=val5),  i can get only one pulse(out_trigx_0) in a pwm period,  is that correct?

0 项奖励
回复

2,062 次查看
PetrS
NXP TechSupport
NXP TechSupport

A1) The PWMX generation is closely related to submodule period. The PWM signals are generated in the following manner.

- The INIT and VAL1 registers define the PWM modulo/period. So the PWM counter counts from INIT to VAL1 and then reinit to INIT again etc.

- The VAL2 resp. VAL3 define the compare value when PWMA goes High resp. Low. 

- The VAL4 resp. VAL5 define the compare value when PWMB goes High resp. Low. 

- The VAL0 defines half cycle reload point and also define the time when PWMX signal is set and the local sync signal is reset.

- The VAL1 also causes PWMX reseting and asserting local sync.

So the usage of PMWA and PWMB signals is easy. The PWMX, if not use as input (for capture feature etc), can generate also the PWM signal but you have to take into account that it represents the local sync signal, which is usually selected as sync source by INIT_SEL bits of CTRL2.

The OCTRL’s POLA, POLB, POLX bits inverts PWMA, PWMB and PWMX polarity.

A2) just set TCTRL = 0x04;             // VAL2 match generate OUT_TRIG0

A3) not sure which “match” you want to use, so lets say VAL3, then

       just set TCTRL = 0x08;              // VAL3 match generate OUT_TRIG1

A4) VALx registers does not enable OUT_TRIG generation, it just defines a position in PWM period when OUT_TRIG pulse is generated if enabled by TCTRL.

Petr

2,063 次查看
yanna
Contributor IV

Hi,

My understanding is belove.

Q1:

   If you select PWMX for output pin, then it is high or low should be determined by Val0 register.

   Following is a figure from MPC5643L RM.

   pastedImage_0.png

Q2&Q3&Q4: You can select the signal (Val0 or Val2 or Val4) to out_trig0_0 signal by configuring TCTRLregister.

pastedImage_2.png

Yanna

2,063 次查看
yanna
Contributor IV

Hi,Peter

I remember that there exists the register which determine out signal high or low when the counter matches the Valx value.

So my original understanding is that Rising and Falling edge signal cann't be selected at the same time.

a few minutes ago, I searched the register , but I cann't find it. is my undrstanding wrong?

I use MPC5643L.

Thanks very much!

Yanna

0 项奖励
回复

2,063 次查看
yanna
Contributor IV

Hi,Petr

Yes,you are right.I have know it.

My understanding : Using rising or falling edge is determined by certain register. I1Re and I1Fe cann't happen at the same time.

Thanks very much!

Yanna

0 项奖励
回复

2,063 次查看
fyw
Contributor IV

yes this is what i think! thank you very much

0 项奖励
回复

2,063 次查看
yanna
Contributor IV

:smileyhappy:

0 项奖励
回复

2,063 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

With the help of the TCTRL you define whether and which compare of VALx register generates the OUT_TRIG0 and OUT_TRIG1 output signals which go to the CTU. The connection of OUT_TRIG0 and OUT_TRIG1 signals to CTU is shown in the Figure 7-9 and the Table 7-29;

It is in the format OUT_TRIGx_y

the Y means the FlexPWM submodule, There are four submodules on FlexPWM (0,1,2 and 3).

The X shows it is either OUT_TRIG0 or OUT_TRIG1 signal.

You may see equivalent PWM_ODD_Y and PWM_EVEN_Y signals (Y corresponds to submodule number). Thus you can match OUT_TRIGX_Y (VAL0/1/2/3/4/5) with bits 14-29 in TGSISR register.

Master Reload and OUT_TRIGx_y signals are generated as very short pulse signal, so the rising and falling edge selection may looks little bit irrelevant. Rising/falling edge selection is more applicable for rest of trigger sources (PWMXn, eTIMER output and external pin).

BR, Petr

0 项奖励
回复

2,063 次查看
fyw
Contributor IV

hi, Petr, thank you for your replying!

what i want to know is "VAL0, VAL2, and VAL4 are used to generate OUT_TRIG0",

how out_trig0 can be generated by val0/2/4,  can you Draw a diagram for this?

PS: i think na yan's answer is right.

if na yan's answer is right, OUT_TRIG0 is generated by val2/3(not val0/2/4),  OUT_TRIG1 is generated by val4/5(not by val1/3/5)

0 项奖励
回复