Hello!
I use the function of MPC5744P :this Flash read operation use mirror small Flash memory logical ddress(0x08F9_8000) with overlay.
//57xx_flasah.ld
MEMORY
{
flash_rchw : org = 0x01000000, len = 0x4
cpu0_reset_vec : org = 0x01000004, len = 0x4
Cal_Data_Flash : org = 0x00F98000, len = 16K /*its mirror Flash address is 0x08F9_0000 to 0x08F9_3FFF*/
m_text : org = 0x01000400, len = 2047K
m_data : org = 0x40000000, len = 368K
Cal_Data_RAM : org = 0x4005C000, len = 16K
local_dmem : org = 0x50800000, len = 64K
}
//57xx_ram.ld
MEMORY
{
SRAM : org = 0x40000000, len = 384K
local_dmem : org = 0x50800000, len = 64K
}
//code below:
#define CALIBRATION_SEG __attribute__ ((section(".CalRefPage")))
uint32_t CALIBRATION_SEG CalRefPara[20]={0,1,2,3,5,6,7,8,9,10,11,12,13,14,15,16,17,18,19};
uint8_t CALIBRATION_SEG g_byCalData = 99;
uint8_t CALIBRATION_SEG g_byCalSaveKey = 12;
#define Calibration_Flash_Start_Addr 0x08F98000
#define Calibration_SRAM_Start_Addr 0x4005C000
#define Calibration_Remap_Size 0x4000
Calibration_RAM_CopyDown((uint32_t *)Calibration_Flash_Start_Addr,(uint32_t *)Calibration_SRAM_Start_Addr,Calibration_Remap_Size);
Flash_OverlayRAM_Calibration_Init();
//while(1) code below
Cal_Flash_Data_Read = *((uint32_t *)Calibration_Flash_Start_Addr);/*get the first calibration data stored on the mirror flash*/
Cal_Flash_Data_Read++;/*increase and write to the OverlyRAM*/
pWokPara = (uint32_t *)Calibration_SRAM_Start_Addr;
*pWokPara = Cal_Flash_Data_Read;
when I run the code,and stop at a time :
RAM memory area:
address 0~3 4~7 8~B C~F
4005c000 0C67057A 00000000 00000001 00000002
............... ............ .......
mirror flash memory area:
address 0~3 4~7 8~B C~F
08F98000 0C67057A 00000000 00000001 00000002
............... ............ .......
flash memory area:
address 0~3 4~7 8~B C~F
00F98000 0C670000 00000000 00000001 00000002
............... ............ .......
Then how can I read the mirror flash data with gloabal variables(such as CalRefPara[0])?
or how can I write the data in mirror flash(0x08F98000~ 0x08F9BFFF) (or ram start at 0x4005c000) to flash memory(0x00F98000~ 0x00F9BFFF)?
code below is reading a global varible:
sJ1939Param.sEMU_MCU_FW3.uOutpMotinvtempact = CalRefPara[0];
Hello Both of you,
I am trying to implement Flash Overlay (remapping to SRAM) from 0x00FF0000 Flash memory region to 0x4001FF00 RAM of MPC5744P.
It is not working for me, then i have verified Data sheet, there i can see all the Flash regions are mentioned as "No Overlay".
I am referring this Document "MPC5744P Reference Manual, Rev. 6, 09/2015 ".
Could you explain me the concept behind this ?
i have attached the Register used below
PFLASH_PFCRCR = 0x00000011;
PFLASH_PFCRDE = 0x80000000;
PFLASH_PFCRD0_Word0 = 0x00FF0000;
PFLASH_PFCRD0_Word1 = 0x4001FF00;
PFLASH_PFCRD0_Word2 = 0xFFFF0005;
Hi,
you got expected result. When overlay is turned on, you can see the effect only in mirrored address space. Flash in normal address space is not affected by overlay. You will always read original data from normal address space. So, the calibration data should be read from mirrored address space. If the overlay is turned off, you will read original flash data, if it is turned on, you will read RAM data. Still from the same address (mirrored flash address). And if you want to update the calibration data in flash, normal flash needs to be reprogrammed by yourself.
Regards,
Lukas
Hello!
If I want to get a varible such as CalRefPara[0](value changed from 12 to 100),How can I get the changed value(100)? sJ1939Param.sEMU_MCU_FW3.uOutpMotinvtempact = CalRefPara[0]; The address of CalRefPara[0] is in original flash. Must I get the changed value at the RAM or mirror flash address?