mpc5777 Quadrature mode setting like this?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mpc5777 Quadrature mode setting like this?

464 次查看
Jihoonjkjkjk
Contributor I

I'm using mpc5777 and I'm going to use the encoder A and B with GPIO179, GPIO180. I'm going to use Quadrature mode at this time, but I organized the code as follows. Should I do it like this?

void init_eMIOS_QEDC(void)
{
eMIOS_0.MCR.B.GPREN = 1;
eMIOS_0.MCR.B.GPRE = 0;

//GPIO179 eMIOS_0채널 24
eMIOS_0.UC[24].C.B.MODE = 0x0D; //Quadrature
eMIOS_0.UC[24].C.B.BSL = 0x03; // Internal counter
eMIOS_0.UC[24].C.B.EDSEL = 1;

//GPIO180 eMIOS_0채널 25
SIU.PCR[179].R = 0x0600; // Configure GPIO179 for eMIOS0 (A-phase)
SIU.PCR[180].R = 0x0600; // Configure GPIO180 for eMIOS1 (B-phase)

if(eMIOS_0.UC[24].S.B.OVFL==1)
{
OVFLG += 1;
eMIOS_0.UC[24].S.B.OVFL=1;
}

Counter = eMIOS_0.UC[24].CNT.R;
// Counter = eMIOS_0.UC[24].A.R;
}

The counting value is eMIOS_0.UC[24].CNT.R This one or eMIOS_0.UC[24].A.R; Where is this saved?

 

0 项奖励
回复
1 回复

449 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if GPIO179, GPIO180 are going to be used, eMIOS_0 ch 0 and ch1 are available on those pins. Thus eMIOS_0 ch1 have to be set to QDEC mode, not ch 24 you have. Counting value is read from eMIOS_0.UC[1].CNT.R register.
Moreover you will need to configure IGF module, otherwise inputs does not pass to eMIOS module. See more in 
https://community.nxp.com/t5/MPC5xxx/How-to-setup-eMIOS-QDEC-function/m-p/905051

BR, Petr

0 项奖励
回复