eTimer oflag question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eTimer oflag question

934 Views
大大许
Contributor III

Hi,

I meet some question about eTimer module in mpc57xx mcu ,In the compare registor and oflag operate chapter show oflag state can only change state after count reach compare value.

I want make eTimer1_ETC5 io output an square wave in countine counter mode,

So i set eTimer1_ETC5 io as eTimer input/output functon,eTimer as counter mode ,every 10ms toggle oflag state,but i capture eTimer1_ETC5 output waveform is noncorrect. waveform period is 20ms is right,but  waveform voltage just 1.2V and it shape is not a square waveform.

Labels (1)
4 Replies

794 Views
大大许
Contributor III

Hi,

i want to use eTimer create an event to triggle adc convert,how should i do.

I need to connect eTimer output with adc channel?

0 Kudos
Reply

794 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

The ADC can be directly triggered from eTimer output, usually the channel 5 is used for this purpose.

Below is internal connection of the MPC5744P

 pastedImage_1.png

 

The ADC must enable external trigger and injected conversion.

 

Attached you have an example which shows ADC triggering from the eTimer1 module.

The OFLAG signal from the eTimer1 channel 5 is fed into ADC, and so ADC is set up for injected conversion with end of scan interrupt. Example was done for MPC5604P, but the modules are similar.

BR, Petr

794 Views
大大许
Contributor III

Hello ,

I have some question about adc triggle dma transfer. ADC0 module is configure to one_shot conversion and adc0-ch7 ,adc0-ch8 is enable ,throughout set start flag triggle adc conversion.

when ch7 and ch8 has an eoc condition to triggle dma transfer.

uint32_t adc0ChannelData[64] = {0};

DMAMUX_0.CHCFG[4].B.TRIG = 0;
 DMAMUX_0.CHCFG[4].B.SOURCE = 0x12;
 DMAMUX_0.CHCFG[4].B.ENBL = 1;


 DMA_0.CR.B.CX = 0;      //normal operate mode
 DMA_0.CR.B.ECX = 0;
 DMA_0.CR.B.GRP1PRI = 1;    //Fixed priority arbitration
 DMA_0.CR.B.GRP0PRI = 0;
 DMA_0.CR.B.EMLM = 1;      //enable minor loop mapping and disable offset
 DMA_0.CR.B.CLM = 0;
 DMA_0.CR.B.HALT = 0;
 DMA_0.CR.B.HOE = 0;
 DMA_0.CR.B.ERGA = 0;
 DMA_0.CR.B.ERCA = 0;
 DMA_0.CR.B.EDBG = 0;

  DMA_0.DCHPRI[4].R  = 0x04; /* Grp 0 chan 04, no suspension, no premption */

 DMA_0.TCD[4].SADDR.R = 0xFBE0011C;   //ADC0_CH7_CH8_CDR_ADD
    DMA_0.TCD[4].ATTR.B.SMOD = 0;
    DMA_0.TCD[4].ATTR.B.SSIZE = 2;       //uint32
  DMA_0.TCD[4].SOFF.R = 4;
 DMA_0.TCD[4].SLAST.R = 0;
 
 DMA_0.TCD[4].DADDR.R = (uint32_t) adc0ChannelData;
 DMA_0.TCD[4].ATTR.B.DMOD = 0;
 DMA_0.TCD[4].ATTR.B.DSIZE = 2;
 DMA_0.TCD[4].DOFF.R = 4;
 DMA_0.TCD[4].DLASTSGA.R = -256;       //只有在major loop 完成以后才执行这个步骤
 DMA_0.TCD[4].NBYTES.MLOFFNO.B.SMLOE = 0;   //minor loop enable and link-to-link disable
 DMA_0.TCD[4].NBYTES.MLOFFNO.B.DMLOE = 0;   //minor loop offset is applied to the SADDR

 DMA_0.TCD[4].NBYTES.MLOFFNO.B.NBYTES = 4;           //minor loop cnt

 DMA_0.TCD[4].BITER.ELINKNO.B.ELINK = 0;

 DMA_0.TCD[4].BITER.ELINKNO.B.BITER = 64;
 DMA_0.TCD[4].CITER.ELINKNO.B.ELINK = 0;
 DMA_0.TCD[4].CITER.ELINKNO.B.CITER = 64;

 DMA_0.TCD[4].CSR.B.BWC = 0;
 DMA_0.TCD[4].CSR.B.MAJORLINKCH = 0;
 DMA_0.TCD[4].CSR.B.ACTIVE = 0;
 DMA_0.TCD[4].CSR.B.DONE = 0;
 DMA_0.TCD[4].CSR.B.MAJORELINK = 0;
 DMA_0.TCD[4].CSR.B.ESG = 0;
 DMA_0.TCD[4].CSR.B.INTHALF = 0;
 DMA_0.TCD[4].CSR.B.INTMAJOR = 1;
 DMA_0.TCD[4].CSR.B.START = 0;
 

 DMA_0.ERQ.B.ERQ4 = 1;

I using multiple request to transfer data, I want to make adc0channeldata buffer storing adc0-ch7 and adc0-ch8 data. But i can't make sources address return to initial value when a minor loop completion.How should i do .

Thanks.

0 Kudos
Reply

794 Views
大大许
Contributor III

I'm sorry that i misconfigure  MSCR reg,it lead to waveform it noncorrection

0 Kudos
Reply