I am working on programming the eTPU2 peripheral for the MPC5644A, and I am receiving a linker error.
When I add a simple division statement in C (for example: variable_a = variable_b / variable_c) I receive the following error:
#Error: could not locate symbol '__s32_div_f', required through section...
Looks like a runtime library is required, or something. I cannot find any documentation on runtime libraries with the Freescale eTPU C Compiler. If anyone knows the solution please help. Thanks.
Hello Randall,
Since eTPU doesn’t have signed division instruction, we provide signed division as a library file.
You should include the lib.c file as part of your build.
You can find the library file from eTPU installation directory at : <CW for ETPU v10.x>\ETPU\ETPU_Tools\Command_Line_Tools\lib
Hope it helps.
Stan