eTPU engine 2 on MPC5746

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eTPU engine 2 on MPC5746

681件の閲覧回数
jyothsnarajan
Contributor V

Hi,

I intend to use some channels on eTPU engine 2 on MPC5746. I downloaded the eTPU function sets from NXP website. But all of them use only engine1.

The functions in eTPU_util.c are written such that they can be adapted to run on eTPU engine 1 or engine 2. I tried to use the same examples for eTPU engine 2 by changing the channel numbers on the host side functions and configuring SIUL2 accordingly, but without success.

I have some questions:

1. channel numbers for eTPU engine 2 channels:  Should I use numbers from 32 to 63  or  64 to 95?

each eTPU engine has 32 channels, numbered 0 to 31, so I expect eTPUB channel number to start from 32. But per this macro in etpu_util.h, 

/***************************************************************************//*!* @brief   Channel number expressed by (engine, channel)* @note    All channel numbers for both eTPUs are absolute.*          eTPU_A has channels 0-31 and eTPU_B has channels 64-95.*******************************************************************************/#define FS_ETPU_ENGINE_CHANNEL(x,y) (((x)-1)*64 + y)
eTPUB channel number starts from 64. Why?

2. engine memory size:

In function    uint32_t fs_etpu2_init( struct etpu_config_t p_etpu_config, uint32_t engine_mem_size);

what is engine_mem_size?

3. Do we always have to use and initialize eTPU engine 1? Can my design use only eTPU engine 2?

A simple example that uses engine 2 would be helpful. Does anyone have one to share?

Thank you.

2 返答(返信)

562件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, usually eTPU engines are called eTPU A and eTPU B, on this device for unknown reason they are called eTPU 1 and eTPU2.

It may be confusing a bit as eTPU, eTPU+ and eTPU2 are shortcuts for eTPU architecture i.e. generation (MPC5746R uses eTPU2). What's exactly the case of fs_etpu2_init function - fs_etpu_init initalizes eTPU module, fs_etpu2_init subsequently initializes specific eTPU2-only setting of an eTPU2 module. It is addendum to fs_etpu_init (that is backward compatible with eTPU).

engine_mem_size is related to engine relative addressing mode

Below screenshot from https://www.nxp.com/docs/en/reference-manual/ETPURMAD.pdfpastedImage_1.png

If the engine_mem_size parameter is 0, then such mode in unused.

To point 3) You can use just one engine, but initialization is common for both engines (A and B)

To point 1) eTPU_A has channels 0-31 and eTPU_B has channels 64-95. To be honest I haven't known it why it is so, but I have found an answer:

"It results from the eTPU memory map. The eTPU A channel registers start at address eTPU_base+0x400, eTPU B channel registers at eTPU_base+0x800. This gives a space for 64 channels to each eTPU engine, although there are only 32 channels implemented. The memory map was designed this way in order to keep a possibility of more channels on future devices"

Hope it helps

562件の閲覧回数
jyothsnarajan
Contributor V

Thank you David. That helped.

JoyR

0 件の賞賛
返信