Hi Adrian,
unfortunately there is not TCP/IP stack for S32R247 or MPC5775K compiled in S32 Design Studio. But there is FNET stack ported for PowerPC devices, which you could use. If you are lucky, it will be possible to compile this fnet stack using S32 Design Studio.
Please look at the following application note:
http://cache.nxp.com/assets/documents/data/en/application-notes/AN4577.pdf?fsrch=1&sr=1&pageNum=1
http://cache.nxp.com/assets/documents/data/en/application-notes-software/AN4577SW.zip
I can also provide you ENET driver for MPC5775K (please see attachment of this thread).
Hope it helps.
Regards,
Martin
Hi Adrian,
please look at the figure below:
These are the basic differences. If you need deeper differences, you have to open reference manual and compare the specific things.
If you have any other questions, please feel free to write me back.
Regards
Martin
Hello Adrian,
unfortunately, I have no information about ENET TCP driver.
If you need free solution, the only possibility I see right now is to use FNET stack (it contains also TCP functions) and port it for MPC5775K.
If you can use solution under license, please look at the following links:
PowerPC, TCP/IP Stack | Embedded Tools
TCP/IP Stack Embedded Web Server USNet Ethernet ARM Cortex ColdFire PowerPC USNet No Royalty
Regards,
Martin