when I use freemaster for debugging, there is something wrong .The problem is an USB-CAN driver not found when I try to communicate with the demo.I have installed the USB-CAN driver,who can tell me ,why ?
Hello.
Welcome to the community. I would like to put your question in a forum that may allow it to be better answered by others. However, I will need more information to help the community.
Could you tell us the RTOS you are using, software configuration and board used to help identify? Did it break in a part of the code that you can share of a screen capture of the fault or error?
thanks,
Michael
Thanks a lot .I'm sorry, my english is very poor,I will try to express well.I don't use the RTOS.now I learn the MPC5643L demo ,first I load the correct code with the codewarrior that running properly in the same demo system.when i open the bootloader_demo.pmp ,the interface occours an error which shows in the figure 1.
figure 1 the error that i open the bootloader_demo.pmp
Then I found the reason that theUSB-CAN driver not found,shows in the figure 2.I have installed the driver,but i can't find out why says driver not found .
figure 2 USB-CAN driver not found