We know that PowerPC and ARM are both 32 bits architecture, why PowerPC need 'far' and 'near' but ARM don't?
I used ARM, I never used 'far' and 'near' to tell compiler to distinguish the 24bits address or 32bits address.
I am using MPC5744 now. I put some global variables into an obsalute address in RAM.
variable A adress is 0x40000001;
variable B adress is 0x40040001;
when i copy A to B, I found my project become unsteady. but when i add the '-farcalls' in the compiler commands, it become steady.
So i feel it very strange.
Any body can help me find the reason?
Solved! Go to Solution.
According Power Architecture Build Tools Reference.pdf:
near_abs — objects must be within the range -65,536 bytes to 65,536 bytes
(16 bits on each side)
far_abs — objects must be within the first 32 bits of RAM
Your compiler should warn you if objects are out of range. If they are, you may either use far addressing mode or compiler could have option “Tune relocation”, if enabled, linker the linker will generate so called branch islands what’s should solve the issue as well.
Unfortunately I don’t know how it works with ARM MCUs, I know document comparing ARM with PowerPC, possibly it could help:
https://static.docs.arm.com/dai0245/b/DAI0245B_migrating_from_ppc_to_arm.pdf
According Power Architecture Build Tools Reference.pdf:
near_abs — objects must be within the range -65,536 bytes to 65,536 bytes
(16 bits on each side)
far_abs — objects must be within the first 32 bits of RAM
Your compiler should warn you if objects are out of range. If they are, you may either use far addressing mode or compiler could have option “Tune relocation”, if enabled, linker the linker will generate so called branch islands what’s should solve the issue as well.
Any body help me?